Skip to main content
Associate II
Sep 11, 2026 12:50 PM UTC
Question

LevelX with STM32H573 using FreeRTOS

Hello everyone,

 

I'd like to use the LevelX API with FreeRTOS on an STM32H5 microcontroller.

 

I know that LevelX is typically used with AzureRTOS, but I'd like to know if ST provides any guidance on integrating it with FreeRTOS or if anyone has any suggestions on how I can do this.

 

Thanks for your help.

2 replies

ST Technical Moderator
Sep 11, 2026 3:48 PM UTC

Hi ​@MatheusNifocci77 

You can find this macro LX_STANDALONE_ENABLE to use LevelX standalone.

Update :  You can refer to this STM32 Example library as reference example for STM32C5 using LevelX and FreeRTOS.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
MFARH.1
ST Employee
Sep 17, 2026 8:36 AM UTC

Hello ​@MatheusNifocci77 ,

 

LevelX is now available in the ST GitHub repository as an RTOS-agnostic component.
It now also includes FreeRTOS support under the ports/freertos path.
GitHub - STMicroelectronics/stm32-mw-levelx at 2.1.0 · GitHub

BR,

Maher