Lack of signals Issue in I2C communication on the STM32G0B1RBT6
我现在使用STM32G0B1RBT6的62 63管脚,需要使用他们I2C通讯功能。现在断开这两个端口一切外设,只留下2.2K上拉电阻。为啥示波器上面一直都没有信号,一直都是保持3.3V上拉。但是把这2个端口配置成普通的GPIO又能够电平翻转。
配置成I2C1 发数据,引脚上 测不到时钟信号。
Translation:
I am currently using pins 62 and 63 on the STM32G0B1RBT6 for I2C communication. I have disconnected all external peripherals from these pins, leaving only 2.2kΩ pull-up resistors in place. However, the oscilloscope shows no signal—the line remains held at the 3.3V pull-up level. Interestingly, if I reconfigure these pins as standard GPIOs, I am able to toggle their logic levels.
When I configure them for I2C1 and attempt to transmit data, no clock signal can be detected on the pin.