Skip to main content
Snm.1
Associate III
Mar 26, 2025 12:30 PM UTC
Question

jump function

I have jump function this like that but this method don't work. Please I need help immedietly

void jumpToAddress(uint32_t jump_address)
{
void (*jumpFunction)(void);
static constexpr uint32_t SHIFTED_JUMP_ADDRESS_DUE_TO_RESET_HANDLER = 4;
static constexpr uint8_t NVIC_REGISTER_LENGTH = 8;

SCB_DisableDCache();
SCB_DisableICache();

__disable_irq();

SysTick->CTRL = 0;

HAL_RCC_DeInit();

for (uint8_t i = 0; i < NVIC_REGISTER_LENGTH; i++)
{
NVIC->ICER[i] = 0xFFFFFFFF;
NVIC->ICPR[i] = 0xFFFFFFFF;
}

SCB->VTOR = jump_address;

__set_MSP(*((uint32_t *)jump_address + SHIFTED_JUMP_ADDRESS_DUE_TO_RESET_HANDLER));

jumpFunction = (void (*)(void))(*((uint32_t *)((jump_address + SHIFTED_JUMP_ADDRESS_DUE_TO_RESET_HANDLER))));
__enable_irq();
jumpFunction();

while (1);
}

 

This topic has been closed for replies.

1 reply

mƎALLEm
ST Technical Moderator
Mar 26, 2025 12:31 PM UTC

Hello,

Please use </> button to share your code.

See the tips on this link. I'm editing your post.

Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.