Skip to main content
Visitor II
Nov 29, 2024 4:52 AM UTC
Question

Issue with I2C Communication on Nucleo-L452RE: Master and Slave Indicate BUSY State

Hello,

I am currently working with I2C communication using the Nucleo-L452RE board. I am encountering an issue where:

  1. The master device indicates that the slave is busy receiving.
  2. Simultaneously, the slave device indicates that the master is busy receiving.

I have double-checked the configuration for both devices and ensured that the pull-up resistors are correctly connected. Despite this, the communication remains stuck in a busy state.

Here are some additional details about my setup:

  • Microcontroller: STM32L452RE
  • I2C Role: Master (Nucleo-L452RE), Slave (Nucleo-L452RE)
  • Pull-Up Resistors: [Specify values, e.g., 4.7 kΩ]

I would appreciate any insights or suggestions to resolve this issue. If more details or specific configurations are required, please let me know.

Thank you in advance for your help!

This topic has been closed for replies.

2 replies

ST Employee
Dec 5, 2024 10:51 AM UTC

Hello @kushikundana,

Thank you for your contribution. you can find several helpful I2C examples here: STM32CubeL4/Projects/NUCLEO-L476RG/Examples/I2C at master · STMicroelectronics/STM32CubeL4.

These examples cover various I2C scenarios and can provide valuable insights and reference code for your project.

 

With Regards,

"If your question is answered, please close this topic by clicking ""Accept as Solution""."
Karl Yamashita
Super User
Dec 6, 2024 11:13 PM UTC

Did you check with an oscilloscope to see if the I2C bus isn't in a low state?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source