Skip to main content
Robmar
Senior II
July 14, 2026
Question

Issue in USB_CoreReset() occasionally fails in debug mode H743

On the H743 using V1.12.1 library, CubeIDE,  the USB_CoreReset() procedure occasionally fails to reset the Host USB core in debug mode.  I have added a reset call which seems to fix the issue in debug, reproduced below.
I would like to know if this is a known issue in CubeIDE debug mode?

See fix below in USB_CoreReset()
 

// mod - added extra reset as in debug the USB host core fails to reset correctly at times

static void USB_Hard_Reset(USB_OTG_GlobalTypeDef *USBx)

{

/* Example from USBH_LL_Init() in usbh_conf.c USB_HOST/Target/

__HAL_RCC_USB_OTG_HS_FORCE_RESET();

HAL_Delay(50);

__HAL_RCC_USB_OTG_HS_RELEASE_RESET();

HAL_Delay(50);

/* --- FS BACK-POWER FIX START ---

HAL_PWREx_EnableUSBVoltageDetector();

uint32_t to = 100000;

while (__HAL_PWR_GET_FLAG(PWR_FLAG_USB33RDY) == 0U && to--) ;

assert(to > 0);*/

uint32_t timeout;

/* 1. Mask all interrupts and stop AHB transactions */

USBx->GINTMSK = 0U;

USBx->GAHBCFG &= ~USB_OTG_GAHBCFG_GINT; // disable global int

/* 2. Wait for AHB idle */

timeout = 0xFFFFU;

while (((USBx->GRSTCTL & USB_OTG_GRSTCTL_AHBIDL) == 0U) && (timeout-- > 0U))

{

/* wait */

}

/* 3. Core soft reset */

USBx->GRSTCTL |= USB_OTG_GRSTCTL_CSRST;

timeout = 0xFFFFU;

while (((USBx->GRSTCTL & USB_OTG_GRSTCTL_CSRST) != 0U) && (timeout-- > 0U))

{

/* wait */

}

/* 4. Flush TX FIFOs */

USBx->GRSTCTL = USB_OTG_GRSTCTL_TXFFLSH | (0x10U << 6); // all TX FIFOs

timeout = 0xFFFFU;

while (((USBx->GRSTCTL & USB_OTG_GRSTCTL_TXFFLSH) != 0U) && (timeout-- > 0U))

{

/* wait */

}

/* 5. Flush RX FIFO */

USBx->GRSTCTL = USB_OTG_GRSTCTL_RXFFLSH;

timeout = 0xFFFFU;

while (((USBx->GRSTCTL & USB_OTG_GRSTCTL_RXFFLSH) != 0U) && (timeout-- > 0U))

{

/* wait */

}

/* 6. Clear pending core interrupts */

USBx->GINTSTS = 0xFFFFFFFFU;



/* 7. Leave core in clean, disabled state.

Higher-level init (host/device, FIFOs, GCCFG, etc.) must be redone after this. */

}



Affected stock HAL routine:-

/**

* @brief Reset the USB Core (needed after USB clock settings change)

* @param USBx Selected device

* @retval HAL status

*/

static HAL_StatusTypeDef USB_CoreReset(USB_OTG_GlobalTypeDef *USBx)

{

#ifdef DEBUG // mod - added to overcome debug mode HOST HS core hang

USB_Hard_Reset(USBx);

#endif

__IO uint32_t count = 0U;

/* Wait for AHB master IDLE state. */

do

{

count++;

if (count > HAL_USB_TIMEOUT)

{

return HAL_TIMEOUT;

}

} while ((USBx->GRSTCTL & USB_OTG_GRSTCTL_AHBIDL) == 0U);

/* Core Soft Reset */

count = 0U;

USBx->GRSTCTL |= USB_OTG_GRSTCTL_CSRST;

do

{

count++;

// BUG IN DEBUG MODE?? SOMETIMES TIMES-OUT IN DEBUG MODE THEM USB HOST FAILS TO WORK

if (count > HAL_USB_TIMEOUT)

{

return HAL_TIMEOUT;

}

} while ((USBx->GRSTCTL & USB_OTG_GRSTCTL_CSRST) == USB_OTG_GRSTCTL_CSRST);

return HAL_OK;

}

 

1 reply

Robmar
RobmarAuthor
Senior II
July 14, 2026

This article seems to relate though gives no hard fix:

FAQ: Troubleshooting a USB core soft reset stuck on an STM32 | Community