Skip to main content
JLojo
Associate III
Jun 6, 2019 5:46 PM UTC
Question

Is VCP diver able to handle several devices on Windows 10?

Hello,

I'm using VCP to communicate with an STM32F303 device, which works well.

However, when I plug a second device on the same computer, it fails to enumerate properly with the message 'This device cannot start. (Code 10)'.

Is that a known issue?

Is there a way to connect several STM32 on the same computer?

Thanks

jyl

This topic has been closed for replies.

4 replies

waclawek.jan
Super User
Jun 6, 2019 6:11 PM UTC

And if you unplug the first device and plug in the second one?

Don't they draw excessive power?

JW

JLojo
JLojoAuthor
Associate III
Jun 6, 2019 10:32 PM UTC

Both work perfectly as long as they are alone on the computer...

jyl

Pavel A.
Jun 6, 2019 8:37 PM UTC

Non unique "serial number" ?

-- pa

JLojo
JLojoAuthor
Associate III
Jun 6, 2019 10:30 PM UTC

Hmm, maybe same ID...

I thought serial number was assigned automatically for each device...

I'll check this in mode details.

Thanks Pavel!