Skip to main content
Senior
Nov 21, 2024 11:17 PM UTC
Solved

Is TXP Necessary for SPI Slave?

I am having issues with my slave responding to my master. I am trying to lessen complexity by only using RXP on the slave, without TXP. The slave (Nucleo-H743ZI) responds one byte late.

On the CS interrupt I send 0 for the first byte and enable RXP.

*((__IO uint8_t *)&hspi1.Instance->TXDR) = 0;
__HAL_SPI_ENABLE_IT(&hspi1, SPI_IT_RXP);
__HAL_SPI_ENABLE(&hspi1);

I then receive a byte and set the next transmit byte. I use FPint so the master does not send data when it is low (used for later implementation).  

void spiISRSTM(SPI_HandleTypeDef *hspi) {

	//Receive if ready
	if (hspi->Instance->SR & SPI_FLAG_RXP) {
		HAL_GPIO_WritePin(nFPINT_GPIO_Port, nFPINT_Pin, GPIO_PIN_RESET);	
 	rxBuffer = (*(__IO uint8_t *)&hspi->Instance->RXDR);
 	(*(__IO uint8_t *)&hspi->Instance->TXDR) = 1;
 	HAL_GPIO_WritePin(nFPINT_GPIO_Port, nFPINT_Pin, GPIO_PIN_SET);

	}
	__HAL_SPI_CLEAR_UDRFLAG(hspi);
	__HAL_SPI_CLEAR_OVRFLAG(hspi);
	__HAL_SPI_CLEAR_EOTFLAG(hspi);
	__HAL_SPI_CLEAR_FREFLAG(hspi);

}

The MISO line for this setup is:

0011 1111

I would expect:

0111 1111

Any Ideas what is causing this?

This topic has been closed for replies.
EthanMankinsBest answer
Senior
Nov 25, 2024 10:27 PM UTC

The issue was an underrun after the first byte. Disabling and reenabling spi after read and before transmit solved the issue.

sr = hspi->Instance->SR;
if ((sr & (SPI_FLAG_RXP | SPI_FLAG_TXC)) == (SPI_FLAG_RXP | SPI_FLAG_TXC)) {
		HAL_GPIO_WritePin(nFPINT_GPIO_Port, nFPINT_Pin, GPIO_PIN_RESET);	//Lower nFPINT
		rxBuffer = (*(__IO uint8_t *)&hspi->Instance->RXDR);
		__HAL_SPI_DISABLE(&hspi1);
		__HAL_SPI_ENABLE(&hspi1);
		pPacketSlave->ProcessSPI();
		(*(__IO uint8_t *)&hspi->Instance->TXDR) = txBuffer;
	}

4 replies

ST Technical Moderator
Nov 22, 2024 10:26 AM UTC

Hello @EthanMankins 

Could you try activating DXP interrupt and checking on DXP flag instead of RXP? 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Senior
Nov 22, 2024 4:42 PM UTC

Hi @Saket_Om 

I have tried this and it does not make difference to the timing.

EthanMankinsAuthorBest answer
Senior
Nov 25, 2024 10:27 PM UTC

The issue was an underrun after the first byte. Disabling and reenabling spi after read and before transmit solved the issue.

sr = hspi->Instance->SR;
if ((sr & (SPI_FLAG_RXP | SPI_FLAG_TXC)) == (SPI_FLAG_RXP | SPI_FLAG_TXC)) {
		HAL_GPIO_WritePin(nFPINT_GPIO_Port, nFPINT_Pin, GPIO_PIN_RESET);	//Lower nFPINT
		rxBuffer = (*(__IO uint8_t *)&hspi->Instance->RXDR);
		__HAL_SPI_DISABLE(&hspi1);
		__HAL_SPI_ENABLE(&hspi1);
		pPacketSlave->ProcessSPI();
		(*(__IO uint8_t *)&hspi->Instance->TXDR) = txBuffer;
	}