Skip to main content
BBert
Associate III
Apr 23, 2022 1:57 PM UTC
Question

Is there an example USB HID host that supports both a mouse and a keyboard at the same time?

..

This topic has been closed for replies.

6 replies

Pavel A.
Apr 23, 2022 10:10 PM UTC

Are your mouse and keyboard separate devices connected to two USBH controllers, or one multifunction (composite) device, or you want to use one USBH controller with a hub?

In the former case you can combine the keyboard and mouse examples, on two USB controllers.

ST has long ago promised hub support, but AFAIK still not there. Look at github, especially https://github.com/hathach/tinyusb.

For composite device examples, look on github.

Note that many mice found in the wild are multifunction, with several vendor specific functions of unknown purpose. Many have complicated report format (more than 8 bits of X/Y/scroll, extra buttons...). Examples usually support only simple fixed report format rather than do full parsing of report descriptor.

​

BBert
BBertAuthor
Associate III
Apr 24, 2022 4:14 AM UTC

It is the second (one multifunction composite device). In fact, it is a wireless Ritek Rii model i4 device with a USB dongle that connects to the HID host. I will check the tiny-USB site but the last time I looked they didn't support the HID host.

Pavel A.
Apr 24, 2022 10:52 AM UTC

Then you need to parse the descriptors and find the endpoint numbers for kbd and mouse, and the report format. Keyboards tend to be more standard, mice can surprise.

If you want to work with only this device, you can capture the descriptors and parse offline.

Then use the endpoint numbers to read the reports, as in the examples. Keyboard, then mouse.

BBert
BBertAuthor
Associate III
Apr 24, 2022 2:12 PM UTC

Thanks for the response. The problem I have is I don't understand how to get the example code to talk to both the devices at the same time. The example code will talk to either the mouse or the keyboard but not both. I am already parsing the descriptors and finding the endpoints. I have implemented an alternative approach using a MAX3421e based board, However, I would rather use the sth32H743 USB port to access the device.