Skip to main content
Steven Keeter
Associate III
September 27, 2018
Question

Is there an application note and or sample code showing how to configure and use the on-board PTPV2 (Precision Time Protocol)?

  • September 27, 2018
  • 2 replies
  • 697 views

I am using an ST32F7 device that incorporates IEEE 1588 hardware within the core. I need to know if this functionality is already within the HAL drivers, etc.... and if there is an app note or sample project available. I see discrete steps for masking register bits, etc... within the user's guide, but was hoping that there are already drivers written to handle these steps.

This topic has been closed for replies.

2 replies

ST Technical Moderator
October 3, 2018

Hello @SKeeter​ ,

Unfortunately, we don't have in our plan to implement PTP feature and there is no PTP example or application note available for STM32F7.

The request is already raised internally to implement this feature. But, Currently, not at the short term planning.

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Tesla DeLorean
Guru
October 3, 2018

@STM Community​  Please STOP putting IEEE-1588 references in every diagram for these devices, these are the types of issues that lose you customers and frustrate the others.

I don't see that the F7 implementation would be materially different from the F2/F4 devices which by any reasonable analysis have close to 8 years of history behind them.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..