Skip to main content
AMurr
Visitor II
November 8, 2018
Question

Is there a work-around to mitigate why SDMMC/FATFS cube generated code does not work (V4.27.0) with STM32F769 MCUs?

  • November 8, 2018
  • 0 replies
  • 429 views

The f_mount() function initially returns FR_NOT_READY then on subsequent attempts to mount the SD card the f_mount() function returns FR_DISK_ERR.

There seems to be a lot of posts with a similar (or same) problem on the STM32F4.

I have followed several "suggested" fixes for these but none work.

I have tried both using and not using DMA - the results are the same.

Initially I was developing on a bespoke PCB with an STM32F769BI MCU but decided to try out a very simple project on the STM32F679i-Disco board. Both have the same issue.

FATFS configuration using the default settings

SDMMC1 Clock set to 48MHz - I have tried several clock divide factors

I've also tried using pull-ups on D0..D3 (and without pull ups also)

code snippet from the most simplest of projects...

//declared at global filescope

FATFS myFatFS;

FIL myFile;

UINT testByte;

MX_FATFS_Init();

if(f_mount(&myFatFS, SDPath, 1)==FR_OK)

{

HAL_GPIO_TogglePin(LD_USER2_GPIO_Port, LD_USER2_Pin);

char myPath[] = "WRITE1.TXT\0";

f_open(&myFile, myPath, FA_WRITE | FA_CREATE_ALWAYS);

char myData[] = "Hello World\0";

f_write(&myFile, myData, sizeof(myData), &testByte);

f_close(&myFile);

HAL_Delay(1000);

}

else

{

HAL_GPIO_TogglePin(LD_USER1_GPIO_Port, LD_USER1_Pin);

}

Any help will be gratefully received.

Andy

This topic has been closed for replies.