Skip to main content
JVand.12
Associate II
Apr 2, 2022 4:47 PM UTC
Question

Is there a socket allocation problem with X-CUBE-CELLULAR V7.0 using Azure RTOS and the STM32L462RE discovery kit Cellular IOT board?

In this loop the mqtt client is created, connected and as long as the mqtt server/broker is up, the client continues processing messages. But when the remote mqtt server/broker is manually shut down, and after the timeout expires, nxd_mqtt_client_connect is called repeatedly. For the first six iterations it acquires socket descriptors starting with the value of 0 and that increases to 5. There are only 6 sockets available in the Murata modem. After that the socket descriptor is not correct. The mqtt client cannot reconnect when the remote mqtt server/broker is again started.

*************************** Trace ****************

client disconnected from server

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 0 

LOG ERROR #7: channel=1 / errorId=7 / gravity=2

com connect status 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 1 

LOG ERROR #8: channel=1 / errorId=7 / gravity=2

com connect status 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 2 

LOG ERROR #9: channel=1 / errorId=7 / gravity=2

com connect status 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 3 

LOG ERROR #10: channel=1 / errorId=7 / gravity=2

com connect status 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 4 

LOG ERROR #11: channel=1 / errorId=7 / gravity=2

com connect status 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 5 

LOG ERROR #12: channel=1 / errorId=7 / gravity=2

com connect status 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

***************** Loop fragment ********

while (1) {

 switch (state) {

case 0:

/* Wait Link/Data is enabled before to do/send data on network. */

status = nx_ip_interface_status_check(p_IpInstance, 0U, NX_IP_LINK_ENABLED, &link_status,

 10000); /* 3); => MISRAC2012-Rule-7.2 */

if (status == (UINT)NX_SUCCESS)

{

state = 2;

}

case 1:

t4 = HAL_GetTick();

if ((t4-t3)>(1*10*1000)) {

t3 = HAL_GetTick();

state = 2;

}

break;

case 2:

(void)printf("App starting MQTT creation\n\r");

status = nxd_mqtt_client_create(&mqtt_client, "my_client",

CLIENT_ID_STRING, STRLEN(CLIENT_ID_STRING), p_IpInstance, p_AppPool,

(VOID*)mqtt_client_stack, sizeof(mqtt_client_stack),

MQTT_THREAD_PRIORTY, NX_NULL, 0);

if (status == NXD_MQTT_SUCCESS) {

nxd_mqtt_client_login_set(&mqtt_client,

MQTTNAME, STRLEN(MQTTNAME),

MQTTPASS, STRLEN(MQTTPASS));

/* Register the disconnect notification function. */

nxd_mqtt_client_disconnect_notify_set(&mqtt_client, my_disconnect_func);

/* Create an event flag for this demo. */

ev_status = tx_event_flags_create(&mqtt_app_flag, "my app event");

server_ip.nxd_ip_version = 4;

server_ip.nxd_ip_address.v4 = MQTT_SERVER_ADDRESS;

state = 3;

t5 = HAL_GetTick();

}

break;

case 3:

/* Start the connection to the server. */

(void)printf("Trying to connect MQTT broker\n\r");

nxd_mqtt_client_login_set(&mqtt_client,

MQTTNAME, STRLEN(MQTTNAME),

MQTTPASS, STRLEN(MQTTPASS));

status = nxd_mqtt_client_connect(&mqtt_client, &server_ip, NXD_MQTT_PORT,

MQTT_KEEP_ALIVE_TIMER, 0, 10000);//NX_WAIT_FOREVER

(void)printf("MQTT connect status %u \n\r", status);

if (status == NXD_MQTT_SUCCESS || status == NXD_MQTT_ALREADY_CONNECTED) {

/* Subscribe to the topic with QoS level 0. */

nxd_mqtt_client_subscribe(&mqtt_client, TOPIC_NAME2, STRLEN(TOPIC_NAME2),

QOS0);

/* Set the receive notify function. */

nxd_mqtt_client_receive_notify_set(&mqtt_client, my_notify_func);

state = 4;

break;

} else if (status == NXD_MQTT_CONNECTING) {

state = 3;

break;

}

else {

t6 = HAL_GetTick();

if ((t6-t5)>(1*15*1000)) {

nxd_mqtt_client_delete(&mqtt_client);

state = 2;

t5 = HAL_GetTick();

break;

}

}

*/

break;

case 4:

/* Publish a message with QoS Level 1. */

state = 6;

t2 = HAL_GetTick();

if ((t2-t1)>(1*30*1000)) {

t1 = HAL_GetTick();

(void)printf("MQTT publishing start \n\r");

status = nxd_mqtt_client_publish(&mqtt_client, TOPIC_NAME,

STRLEN(TOPIC_NAME), (CHAR*)MESSAGE_STRING,

STRLEN(MESSAGE_STRING), 0, QOS1, 10000);

(void)printf("MQTT publish status %u \n\r", status);

if (status == NXD_MQTT_SUCCESS) {

state = 6;

} else

{

state = 3;

t5 = HAL_GetTick();

}

}

tx_event_flags_get(&mqtt_app_flag, DEMO_ALL_EVENTS,

TX_OR_CLEAR, &events, 5000);

break;

case 5:

break;

case 6:

if(events & DEMO_MESSAGE_EVENT)

{

nxd_mqtt_client_message_get(&mqtt_client, topic_buffer,

sizeof(topic_buffer), &topic_length, message_buffer,

sizeof(message_buffer), &message_length);

topic_buffer[topic_length] = 0;

message_buffer[message_length] = 0;

printf("topic = %s, message = %s\n\r", topic_buffer, message_buffer);

}

state = 4;

break;

 }

 }

This topic has been closed for replies.