Skip to main content
gerhard
Associate III
Mar 3, 2021 2:53 PM UTC
Solved

Is there a FreeRTOS demo program for F4 or L4 ?

Is there a FreeRTOS demo program, using STM32CubeMX to set up, for:

STM3240G-EVAL - EVAL with STM32F407IG MCU or

STM32L476G-EVAL with STM32L476ZGT6 or

STM32F429IDISCOVERY with STM32F429ZIT6

Any help appreciated

 

I want to use STM32CubeMX to set upany of these eval boards, with FreeRTOS enabled, to create FreeRTOS code for testig

 

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Mar 3, 2021 3:33 PM UTC

Hello @gerhard​ ,

There is no .ioc working project for FreeRTOS.

There is a rich set of FreeRTOS applications useful for your case with STM32cube packages that use HAL library and configured for different toolchains: EWARM, MDK-ARM, SW4STM32. 

Try to pick the one suitable for the device and board you are using and start from it:

  • STM32Cube_FW_F4_V1.25.2\Projects\STM324xG_EVAL\Applications\FreeRTOS
  • STM32Cube_FW_L4_V1.16.0\STM32Cube_FW_L4_V1.16.0\Projects\STM32L476G-EVAL\Applications\FreeRTOS

To start with STM32CubeMx, I advise you to refer to the "FreeRTOS" section in the UM1718 STM32CubeMx user Manual.

Have a look also to the UM1722 User manual about "Developing Applications on STM32Cube with RTOS", this will help you on FreeRTOS configuration.

Please mark my answer as the best by clicking the "Select as best" button if it helped you. This will help other users find this solution more quickly.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Imen.DBest answer
ST Technical Moderator
Mar 3, 2021 3:33 PM UTC

Hello @gerhard​ ,

There is no .ioc working project for FreeRTOS.

There is a rich set of FreeRTOS applications useful for your case with STM32cube packages that use HAL library and configured for different toolchains: EWARM, MDK-ARM, SW4STM32. 

Try to pick the one suitable for the device and board you are using and start from it:

  • STM32Cube_FW_F4_V1.25.2\Projects\STM324xG_EVAL\Applications\FreeRTOS
  • STM32Cube_FW_L4_V1.16.0\STM32Cube_FW_L4_V1.16.0\Projects\STM32L476G-EVAL\Applications\FreeRTOS

To start with STM32CubeMx, I advise you to refer to the "FreeRTOS" section in the UM1718 STM32CubeMx user Manual.

Have a look also to the UM1722 User manual about "Developing Applications on STM32Cube with RTOS", this will help you on FreeRTOS configuration.

Please mark my answer as the best by clicking the "Select as best" button if it helped you. This will help other users find this solution more quickly.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
gerhard
gerhardAuthor
Associate III
Mar 4, 2021 3:36 PM UTC

Thanks,

Very helpful information.