Skip to main content
CGran.3
Associate II
Nov 3, 2021 8:39 PM UTC
Question

Is there a complete/correct STM32H73x.svd file anywhere?

I have the STM32H73x.svd from then STMCubeH7 pack version 1.9.0 but it is far from compete/correct.

Some examples

AHB3 clock enable /reset registers do not have any of the OCTOSPI items in there, but has a QSPI entry.

Similar some timer enables/reset are in the same case (23 and 24 specifically)

the Flash ACR register field for Latency is the incorrect length (3 when it should be 4)

This topic has been closed for replies.

18 replies

Nov 4, 2021 7:17 AM UTC

Hello,

I've discovered lately that ST offers most up to date SVD files on the product web page.

In your case it should be https://www.st.com/en/microcontrollers-microprocessors/stm32h723-733.html#cad-resources

Then click on the System View Description link.

I'm not saying it has everything in it, but it should be the latest revision available.

Best regards.

Mike_ST
ST Technical Moderator
Nov 4, 2021 12:54 PM UTC

It is described as 3 bits there as well.

I entered a ticket for this FLASH->ACR.Latency mismatch (refman vs svd).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
CGran.3
CGran.3Author
Associate II
Nov 4, 2021 4:58 PM UTC

@Mike_ST​ 

Can you also put a ticket in to get the enable/reset registers fixed. Specifically the AHB3 ones for OCTOSPI and APB1 for the Timer 23 and 24?

Mike_ST
ST Technical Moderator
Nov 4, 2021 9:05 AM UTC

Hello,

There are some in the STM32CubeProgrammer as well:

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\SVD

I know this is convenient to have them already complete but it can be edited just to add what is missing.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Nov 4, 2021 11:10 AM UTC

Hi @Mike_ST​ ,

While this is true, the files that comes with CubeProgrammer are not up to date.

For example the G0B1RE SVD file that ships with the version 2.8.0 is quite old and uncomplete.

I am not sure that CubeProgrammer needs to have an auto update system integrated (something like git fetch/pull), as it needs to stay slick and reactive...

Best regards.

Mike_ST
ST Technical Moderator
Nov 4, 2021 11:17 AM UTC

>>For example the G0B1RE SVD file that ships with the version 2.8.0 is quite old and uncomplete.

Can you give one example of what is missing ?

I can enter a ticket if I have one.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
JCH
Visitor II
May 30, 2022 12:15 PM UTC

@Mike_ST​ : Could you please also update OTG_HS register description? At least the description of OTG_HS_GOTGCTL is not complete, others probably as well. I'm using an STM32H743. The SVD ist STM32H743.svd which comes from the Keil STM32H7xx_DFP version 3-0-0. It is the same file that can also be downloaded from the ST homepage (CAD section) directly (see above).

Mike_ST
ST Technical Moderator
May 31, 2022 8:15 AM UTC

Ok, I've added that in the ticket.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.