Skip to main content
Vkris.1
Associate II
Aug 25, 2023 6:57 AM UTC
Question

Is it possible to implement secure boot without using trust zone for stm32U585??

Is it possible to implement secure boot without using trust zone for stm32u585.

without trust zone i want to use Boot lock, OTP, secure address like features.

This topic has been closed for replies.

2 replies

Aug 25, 2023 12:18 PM UTC

Hi,

Yes, it is possible to implement secure boot without using TrustZone for STM32U585. The STM32U585 microcontroller supports a range of security features including Boot lock, OTP, and secure address space which can be used to implement secure boot.

The STM32Cube MCU Package provides a Secure Boot and Secure Firmware Update solution for STM32 microcontrollers. This solution is based on the open-source TF-M reference implementation.

Regards

Vkris.1
Vkris.1Author
Associate II
Aug 29, 2023 11:05 AM UTC

Thanks for Response.

I would like to know can we port the SBSFU along with Secure Engine (STM32CubeExpansion_SBSFU_V2.6.2) of STM32H7 series to STM32U5?

The idea is to have a common bootloader for STM32U5 and STM32H7 based on SBSFU package provided for STM32H7(STM32CubeExpansion_SBSFU_V2.6.2) & trying to avoid using TF-M based package, since STM32H7 doesn't support TF-M