Skip to main content
Tbill.1
Associate
Nov 26, 2021 2:36 PM UTC
Solved

Is current-limited power switch needed inOTG_HS "peripheral only" design ?

It 's seem to me there is an error page 2651 of RM0468, STMH730 reference manual.

the figure 782 has a Current limited power switch in the design, but if un understand corretly, is only need in OTG host or dual role device.

Am I correct ? there is no need of current limited power switch on Vbus in peripheral only ?

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Nov 26, 2021 2:40 PM UTC

Welcome, @Tbill.1​, to the community!

Yes, you are right. It is also mentioned in the caption:

1. (Instead) Use a regulator to build a bus-powered device.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Nov 26, 2021 2:40 PM UTC

Welcome, @Tbill.1​, to the community!

Yes, you are right. It is also mentioned in the caption:

1. (Instead) Use a regulator to build a bus-powered device.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.