Skip to main content
Explorer
May 8, 2025 7:02 PM UTC
Solved

Is checking return value of HAL_Transmit/Receive_IT overkill?

Hello everyone, I have a lot (too much) question regarding code optimisation, the safety of a code and some return value of the HAL.

Firstly, I am currently using HAL and CMSIS RTOS v2.  I am using a spi bus protected with a mutexe. Assuming that I am correctly using the mutexe, is it possible for HAL_Transmit_IT or HAL_Receive_IT to actually return HAL_Busy?

What I want to know is:

1) Am I making too much verification? Afterall a if/else bloc is require some ressources from the core, even if it's very little.

2) I read on various post that using assert was a good practice in embbeded system but I'm still strugling to know when to use it and when not. I also read that it was recommanded to always check a return value of a function when it has one. 

Am I using correctly the assert() function? Is there too much usage of it? Not enough? Where is it really required and when is it not?



Here is a sample of a basic function for a driver I am currently working on. I'm following the same code structure in all my other function so it gives a good idea of how I use insert and HAL return checking in other parts of my code.

osStatus_t ADXL375_set(ADXL375_handler_t* handler, ADXL375_register_t register_adress, uint8_t new_data) {
	//Parameter check
	assert(handler != NULL);

	osStatus_t driver_status = osMutexAcquire(handler->spi_mutex, osWaitForever);
	if (driver_status == osOK) {
		uint8_t command[2];
		command[0] = register_adress;
		command[1] = new_data;
		HAL_GPIO_WritePin(handler->cs_gpio, handler->cs_pin, GPIO_PIN_RESET);
		HAL_StatusTypeDef spi_status = HAL_SPI_Transmit_IT(handler->hspi, command, 2);
		if (spi_status == HAL_OK) {
			driver_status = osOK;
			//The flag tell the system that it is this driver that used the SPI bus.
			osEventFlagsSet(handler->read_sensors_event, handler->event_flag_number);
		} else {
			//Should never return HAL busy or error since parameter are checked and mutex is used.
			assert(0);
		}
	} else {
		//Error on Mutex. It should not happend so I guess it is critical enough to restart the program?
		assert(0);
	}
	return driver_status;
}

 
Don't hesistate to tell me if my question is unclear or if it needs precision.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 8, 2025 10:04 PM UTC

Depends if you want to be able to diagnose failure when it occurs.

The _IT and _DMA calls can only have a single instance "in-flight" at any given time, so you have to catch those failures, or errors sent to the callbacks, etc. There can be multiple exit paths, so if you get out-of-sync you could end up with a situation where communications stall or just stop completely. Basically a resource leak.

asserts can be good for a debug/diagnostic build as they can catch a lot of parameter passing errors. Probably too much for a customer release.

Customer States "Doesn't Work"  : From a support perspective getting no feedback on the cause/nature of a failure is very unhelpful.

You'll have to decide at what level you want to catch and report errors, having HardFault_Handler() and Error_Handler() provide some context will help. On the other hand reporting every HAL interaction, might be too much, but you want it to propagate the error upward, to a point where you can report it, or attempt recovery.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 8, 2025 10:04 PM UTC

Depends if you want to be able to diagnose failure when it occurs.

The _IT and _DMA calls can only have a single instance "in-flight" at any given time, so you have to catch those failures, or errors sent to the callbacks, etc. There can be multiple exit paths, so if you get out-of-sync you could end up with a situation where communications stall or just stop completely. Basically a resource leak.

asserts can be good for a debug/diagnostic build as they can catch a lot of parameter passing errors. Probably too much for a customer release.

Customer States "Doesn't Work"  : From a support perspective getting no feedback on the cause/nature of a failure is very unhelpful.

You'll have to decide at what level you want to catch and report errors, having HardFault_Handler() and Error_Handler() provide some context will help. On the other hand reporting every HAL interaction, might be too much, but you want it to propagate the error upward, to a point where you can report it, or attempt recovery.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..