Skip to main content
magene
Senior
Dec 14, 2023 11:31 PM UTC
Solved

IRQ Handlers with LL drivers

I generally prefer the STM Low Level drives and chose that driver family for most peripheral in CubeMX Project Manager->Advanced Settings->Driver Selector.  There seem to be one disadvantage: the IRQHandlers are not generated as weak which I think happens with the CubeMX generated HAL IRQHandlers.  So with the LL drivers, I have to add a line of code to the CubeMX generated stm32h7xx_it.c file.  Like this:

 

 

 

 

void USART1_IRQHandler(void)
{
 /* USER CODE BEGIN USART1_IRQn 0 */
 myUSART1_IRQHandler();
 /* USER CODE END USART1_IRQn 0 */
 /* USER CODE BEGIN USART1_IRQn 1 */

 /* USER CODE END USART1_IRQn 1 */
}

 

 

 

 

Is there a way to tell CubeMX to generate the IRQHandler stubs as weak?

And what does the CubeMX Project Manager->Advanced Settings->Register CallBack disable/enable setting do? I've generated code with this enabled and disabled and don't see any obvious difference.

Thanks

This topic has been closed for replies.
TDK
TDKBest answer
Dec 15, 2023 6:19 PM UTC

Yes, those are effectively your options.

The HAL has its own callbacks for transfer complete, or when a character is received, or whatever. I would implement and use those if you don't need computational speed.

If you do need computational speed, I would add the user code to the IRQ function in stm32_*_it.c directly. Calling your own function in there with user code is also fine, but will be a little slower.

 

Really up to you, no wrong method.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

TDK
Dec 15, 2023 4:50 PM UTC

IRQ handlers are never generated as weak--not in HAL or LL.

> Is there a way to tell CubeMX to generate the IRQHandler stubs as weak?

There are weak definitions in startup_*.s file that would conflict with any other weak definitions, so this is not a possibility.

The callback stuff has to deal with how HAL handles callbacks within its machinery, not how IRQ handlers are defined. Not going to help you here.

"If you feel a post has answered your question, please click ""Accept as Solution""."
magene
mageneAuthor
Senior
Dec 15, 2023 5:18 PM UTC

@TDK Thanks for the help. Given that information, it seems like I have 2 options.  Keep doing what I'm doing by adding a line of code to every IRQHandler in the stm32H7xx_it.c file that CubeMX generates. Or remove stm32H7xx_it.c from my project and write my own.

A better question is how would you handle this situation?

Thanks again

TDK
TDKBest answer
Dec 15, 2023 6:19 PM UTC

Yes, those are effectively your options.

The HAL has its own callbacks for transfer complete, or when a character is received, or whatever. I would implement and use those if you don't need computational speed.

If you do need computational speed, I would add the user code to the IRQ function in stm32_*_it.c directly. Calling your own function in there with user code is also fine, but will be a little slower.

 

Really up to you, no wrong method.

"If you feel a post has answered your question, please click ""Accept as Solution""."