Intermittent TCP communication with KSZ8863 broken?
- October 9, 2025
- 5 replies
- 486 views
On a couple of internally developed boards based on an architecture combining an STM32F407 and a KSZ8863RLL, I have experienced failures on the latter chip that I cannot explain. The issue manifests as intermittent communication with the TCP client that pings the board. Occasionally, it seems that some packets are lost, causing the communication to drop out and then resume, only to fail again after a short while. I suspect that the environment in which the board is used might be subject to ESD events or overvoltage conditions caused by imbalances in the differential voltage on the bus. Since we are in an industrial context, it is standard practice to connect the digital grounds of the boards and power supplies to earth. The suspicion that the problem is due to internal damage of the chip is supported by the fact that, on these faulty boards, replacing the KSZ8863 restores normal operation without any interruptions.