Skip to main content
Associate II
May 14, 2025 9:38 AM UTC
Question

Interfacing microphone sensor in STM32H757I-EVAL

Hi, 
I am trying to interface the internal microphone sensor (MP34DT05TR-A) in STM32H757I-EVAL. The goal is to record audio from the MP34DT05 microphones, store it on a microSD card, and play it back on a PC. I'm not able to navigate through this; could you share some resources or the steps that need to be followed to configure this and to record the audio? Also, there are three different data formats: audio codec, DFSDM, and PDM. Which do you think will be suitable for the data acquisition part? 

This topic has been closed for replies.

2 replies

KDJEM.1
ST Technical Moderator
May 14, 2025 11:56 AM UTC

Hello @priya_12;

 

For audio record, I recommend you to start with available examples under STM32CubeH7:

  • \STM32Cube_FW_H7_V1.12.1\Projects\STM32H747I-EVAL\Examples\DFSDM\DFSDM_AudioRecord
  • \STM32Cube_FW_H7_V1.12.1\Projects\STM32H747I-EVAL\Examples\BSP

 

I hope these examples can help you?

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
priya_12Author
Associate II
May 16, 2025 5:48 AM UTC

Hi, 
The first example mentioned is available only with respect to STM32H743I-EVAL. There are some features different in both boards. Could you tell me how to execute this?