Skip to main content
Associate II
Jan 29, 2025 4:27 AM UTC
Solved

Integrating SPI NOR Flash with FATFS and USB MSC

Dear STM Community,

I hope this message finds you well.

I am currently working on a project that involves integrating SPI NOR Flash (MT25TL01GB) with FATFS and USB MSC on STM32F429. Despite my efforts, I have encountered some challenges and would greatly appreciate any guidance or support from the community.

If anyone has experience with this integration or can provide any resources, examples, or advice, it would be immensely helpful.

Thank you in advance for your assistance.

Best regards, [Your Name]

This topic has been closed for replies.
Saket_OmBest answer
ST Technical Moderator
Jan 31, 2025 1:52 PM UTC

@pankaj4 

Please refer to the example in the link below:

STM32CubeF4/Projects/STM32446E_EVAL/Applications/USB_Device/MSC_Standalone at master · STMicroelectronics/STM32CubeF4 · GitHub

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

8 replies

ST Technical Moderator
Jan 29, 2025 1:45 PM UTC

Hello @pankaj4 

Using FatFs with SPI NOR flash is not recommended because the flash memory could fail in a short time, especially with intensive I/O operations like those performed by FatFs. Instead, consider using a more appropriate filesystem library designed for flash memories, such as LittleFS.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
pankaj4Author
Associate II
Jan 30, 2025 6:39 AM UTC

Could you please provide me with an example of how to implement LittleFS with SPI NOR flash? Your guidance would be greatly appreciated.

ST Technical Moderator
Jan 30, 2025 9:30 AM UTC

Hello @pankaj4 

Unfortunately, we don't support it in Cube_FW for the moment, you need to write the API between littlefs & STM32Cube_FW by yourself.

 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
pankaj4Author
Associate II
Jan 31, 2025 12:04 PM UTC

Hi,

Could you please assist me with information on how to operate a NOR flash drive on a PC using USB FS MSC? I came across your post and found the example very helpful, but I need further support with this specific aspect.

Thank you!

Saket_OmBest answer
ST Technical Moderator
Jan 31, 2025 1:52 PM UTC
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om