Skip to main content
Associate
Oct 18, 2023 7:11 AM UTC
Solved

Initialisation of USB_OTG_FS locks up during initialisation on HAL_Delay

When I try to add USB_OTG_FS (host only) to a project which uses FreeRTOS the code locks up on initialisation of USB_OTG_FS.

 

When USB OTG FS is added, a call to "MX_USB_OTG_FS_HCD_Init" is added to "main" function. It goes before a call to "osKernelStart()". During initialisation HAL_Delay is called, and the code locks up on that.

The path looks like this: MX_USB_OTG_FS_HCD_Init >> HAL_HCD_Init >> USB_SetCurrentMode >> HAL_Delay(1U)

And that is where it locks up.

If I comment out the call to "MX_USB_OTG_FS_HCD_Init" the rest works fine. If I put "HAL_Delay" in one of FreeRTOS threads, that works as expected (presumably due to OS being fully functional by that point). If I put "HAL_Delay" just before a call to "osKernelStart()" - it locks up.

It seems that HAL_Delay cannot be called before the call to osKernelStart, and the auto-generated code for initialisation of USB is doing exactly that.

Is it a bug or I am missing something? What would you recommend?

This topic has been closed for replies.
Bob S
Bob SBest answer
Super User
Oct 18, 2023 3:05 PM UTC

This is a known issue with FreeRTOS - calling any function that creates a mutex/queue/task/etc. before osKernelStart() will leave interrupts disabled.  Move the MX_USB_OTG_FS_HCD_Init() call either before MX_FREERTOS_Init()** or inside the default task.

 

** Presuming you have no other init functions that create FreeRTOS entities.

3 replies

Bob S
Bob SBest answer
Super User
Oct 18, 2023 3:05 PM UTC

This is a known issue with FreeRTOS - calling any function that creates a mutex/queue/task/etc. before osKernelStart() will leave interrupts disabled.  Move the MX_USB_OTG_FS_HCD_Init() call either before MX_FREERTOS_Init()** or inside the default task.

 

** Presuming you have no other init functions that create FreeRTOS entities.

rtvdAuthor
Associate
Oct 18, 2023 6:53 PM UTC

Thank you, @Bob S. I have moved it to the default task and now it works fine.

Bob S
Super User
Oct 18, 2023 9:01 PM UTC

Glad it helped.  Feel free to mark my post as "the answer" :)