Skip to main content
Associate II
Nov 20, 2023 8:20 AM UTC
Solved

Init RTC failed - timeout error - stm32wb10cc

hi,

I configure my micro to work on internal clock by cubemx - this is the clock configure:

//#############################################################################################################
//                 Init Device:  System Clock Configuration
//#############################################################################################################
static  void IDM_Config_System_Clock(void)
{
    RCC_OscInitTypeDef RCC_OscInitStruct = {0};
    RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

    /** Initializes the RCC Oscillators according to the specified parameters
    * in the RCC_OscInitTypeDef structure.
    */
    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI1;
    RCC_OscInitStruct.HSIState = RCC_HSI_ON;
    RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
    RCC_OscInitStruct.LSIState = RCC_LSI_ON;
    RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
    if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
    {
      Error_Handler();
    }

    /** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers
    */
    RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK4|RCC_CLOCKTYPE_HCLK2
                                |RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                                |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
    RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
    RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
    RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
    RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    RCC_ClkInitStruct.AHBCLK2Divider = RCC_SYSCLK_DIV1;
    RCC_ClkInitStruct.AHBCLK4Divider = RCC_SYSCLK_DIV1;

    if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
    {
      Error_Handler();
    }
}

and this is the RTC init function:

static void IDM_RTC_Init(void)
{
  RTC_Object.Instance = RTC;
  RTC_Object.Init.HourFormat = RTC_HOURFORMAT_24;
  RTC_Object.Init.AsynchPrediv = 127;
  RTC_Object.Init.SynchPrediv = 255;
  RTC_Object.Init.OutPut = RTC_OUTPUT_DISABLE;
  RTC_Object.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
  RTC_Object.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
   if (HAL_RTC_Init(&RTC_Object) != HAL_OK)
   {
     Error_Handler();
   }
}
but rtc  init is failed, its occured on 

RTC_EnterInitMode() function

 

HAL_StatusTypeDef RTC_EnterInitMode(RTC_HandleTypeDef *hrtc)

{

uint32_t tickstart;

 

/* Check if the Initialization mode is set */

if ((hrtc->Instance->ISR & RTC_ISR_INITF) == 0U)

{

/* Set the Initialization mode */

hrtc->Instance->ISR = (uint32_t)RTC_INIT_MASK;

 

tickstart = HAL_GetTick();

/* Wait till RTC is in INIT state and if Time out is reached exit */

while ((hrtc->Instance->ISR & RTC_ISR_INITF) == 0U)

{

if ((HAL_GetTick() - tickstart) > RTC_TIMEOUT_VALUE)

{

I RECEIVED THE TIMEOUT ERROR HERE:

return HAL_TIMEOUT;

}

}

}

 

return HAL_OK;

}

 

I tried everything without success :(

Can anyone help me to understand where the problem is?

This topic has been closed for replies.
Sarra.SBest answer
ST Employee
Nov 20, 2023 4:54 PM UTC

Hello @aviel, 

Try adding HAL_PWR_EnableBkUpAccess() after SystemClock_Config()

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Sarra.SBest answer
ST Employee
Nov 20, 2023 4:54 PM UTC

Hello @aviel, 

Try adding HAL_PWR_EnableBkUpAccess() after SystemClock_Config()

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
avielAuthor
Associate II
Nov 21, 2023 8:20 AM UTC

Hi Sarra,

thank you!
at now its work for me!

for better understanding why need to add this function?