Skip to main content
JLehm
Associate
May 14, 2019 12:20 PM UTC
Solved

Inconsistent ethernet RX descriptor queue when using context descriptor

The following bug occurs in the stm32h7xx_hal_eth library:

When a feature of the ehernet peripheral is enabled which causes the DMA to use RX context descriptors, for example the ieee1588 timestamping unit, this leads to an inconsistent state of the RX descriptor list.

I discovered that this is caused by the HAL_ETH_BuildRxDescriptors function which does not clear the own bit of the context descriptor and does not reset the context descriptor in the descriptor list.

The following changes solve the problem:

line 1159

if(descscan < (dmarxdesclist->AppDescNbr -1))

needs to be replaced by

if(descscan < (totalappdescnbr - 1))

The line

WRITE_REG(dmarxdesclist->AppContextDesc, 0);

needs to be added before the return statement.

Cheers, Jan

This topic has been closed for replies.
JLehm
JLehmBest answer
Associate
May 22, 2019 11:04 AM UTC

I did not test it, but i had a look at the HAL_ETH_BuildRxDescriptors function in version 1.4.0 and i don't see any changes there. So i guess the bug is not fixed yet.

7 replies

ST Technical Moderator
May 22, 2019 9:15 AM UTC

Hello,

Could you please precise in which version of STM32CubeH7 you have found this issue. So, we can verify it.

Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
JLehm
JLehmAuthor
Associate
May 22, 2019 9:43 AM UTC

Unfortunately we are not able to reliably reconstruct this information, but we are 90% certain that it was STM32Cube H7 V1.3.0.

ST Technical Moderator
May 22, 2019 9:56 AM UTC

Can you please confirm if that problem is still being faced with the latest version of firmware package STM32CubeH7 v1.4.0 ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
JLehm
JLehmAuthorBest answer
Associate
May 22, 2019 11:04 AM UTC

I did not test it, but i had a look at the HAL_ETH_BuildRxDescriptors function in version 1.4.0 and i don't see any changes there. So i guess the bug is not fixed yet.

ST Technical Moderator
May 22, 2019 11:11 AM UTC

Ok, thanks for your reply. We will check this issue internally and come back to you soon with update.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks