Skip to main content
Daniel Hailu
Associate II
August 10, 2017
Question

Implementation on a STM32F407 host mode USB driver, able to connect and communicate with USB serial devices such as Telit?

Posted on August 10, 2017 at 22:09

I was looking for C code and software written that implements a STM32F407 host mode USB driver, able to connect and communicate with USB serial devices that expose multiple virtual devices such as Telit GSM modems.

* Implemented using this GCC ARM toolchain

* Using the standard STM32 USB base USB libraries

* Thread safe, implemented under FreeRTOS reference sample application (we will provide base sample application)

* Each discovered bi-directional stream presented as a stream from the library

* Notify on device connection / disconnections

If you have done this or have library and drivers please reply!

#usb-modem #usb #stm-32f407 #usb-host-vcp
This topic has been closed for replies.