Skip to main content
DCtech
Associate III
February 17, 2021
Question

ICMP-IPv4 total length exceeds packet length

I have a problem with +500byte ICMP packet, I am using ubuntu 16.04 and firewall inactive. When I try to send ping with this command 

ping -s 500 192.168.1.127

 ping is successfull, but when I try to send this 

ping -s 580 192.168.1.8

 ping reply didnt accept from computer but my 192.168.1.127 device send reply I see on network analyser. But computer not accept 500+ data. How can I solve this problem.

When I send the 500+ ping from computer my device replied just one time, and it shows me this error:

Expert Info (Error/Protocol): IPv4 total length exceeds packet length (578 bytes)

enter image description here

and I have bad checksum

What is the reason for the this error ? Pc connected point to point to my stm32+lwip device with ethernet interface.

This topic has been closed for replies.