Senior II
May 7, 2021 2:42 AM UTC
Question
I2S BUS acting weird when using FWS = 196KHz
- 7 replies
- 1950 views
Hi guys, Ill keep this short, anytime I set the I2S bus to use FWS = 196KHz it acts all whack.
I am not sure if its the tool I am measuring with but its a saleae logic analyzer so I doubt it.
Here a picture of what I am talking about
I double checked everything the clock config is correct, I double checked with other FWS work such as 96,48, and 44.1 KHz and they are all fine
The GPIOs are using the "Very High Speed" Setting as well
Code
/*
* AUDIO_SELECTOR_FACTORY.c
*
* Created on: May 3, 2021
* Author: Christopher
*/
#include <CONSTANTS.h>
#include "stm32h753xx.h"
#include "Opcode.h"
void INPUT_AUDIO_SELECTOR (int INPUT_TYPE, int BIT_RATE, int SAMPLING_RATE) {
RCC->APB2ENR |= (RCC_APB2ENR_SPI1EN);
//DECONFIG I2S
DMA1_Stream0->CR &= ~DMA_SxCR_EN;
DMA1_Stream1->CR &= ~DMA_SxCR_EN;
SPI1->CR1 &= ~SPI_CR1_SPE;
SPI1->CR1 &= ~SPI_CR1_CSTART;
RCC -> CR &= ~(RCC_CR_PLL2ON);
//CONFIG I2S
switch (SAMPLING_RATE) {
case 192000:
RCC -> PLLCKSELR &= ~(RCC_PLLCKSELR_DIVM2);
RCC -> PLLCKSELR |= (RCC_PLLCKSELR_DIVM2_DIV10);
RCC -> PLL2FRACR = 0;
RCC -> PLL2FRACR = (RCC_PLL2FRACR_FRACN2_7209);
RCC -> PLLCFGR &= ~((RCC_PLLCFGR_PLL2VCOSEL) |
(RCC_PLLCFGR_PLL2RGE) |
(RCC_PLLCFGR_PLL2FRACEN) |
(RCC_PLLCFGR_DIVP2EN) |
(RCC_PLLCFGR_DIVQ2EN) |
(RCC_PLLCFGR_DIVR2EN));
RCC -> PLLCFGR |= (RCC_PLLCFGR_PLL2VCOSEL_WIDE_RANGE) |
(RCC_PLLCFGR_PLL2RGE_8MHz_16MHz) |
(RCC_PLLCFGR_DIVP2EN) |
(RCC_PLLCFGR_PLL2FRACEN);
RCC -> PLL2DIVR &= ~((RCC_PLL2DIVR_N2) |
(RCC_PLL2DIVR_P2));
RCC -> PLL2DIVR |= (RCC_PLL2DIVR_N2_122) |
(RCC_PLL2DIVR_P2_4);
break;
case 96000:
RCC -> PLLCKSELR &= ~(RCC_PLLCKSELR_DIVM2);
RCC -> PLLCKSELR |= (RCC_PLLCKSELR_DIVM2_DIV10);
RCC -> PLL2FRACR = 0;
RCC -> PLL2FRACR = (RCC_PLL2FRACR_FRACN2_7209);
RCC -> PLLCFGR &= ~((RCC_PLLCFGR_PLL2VCOSEL) |
(RCC_PLLCFGR_PLL2RGE) |
(RCC_PLLCFGR_PLL2FRACEN) |
(RCC_PLLCFGR_DIVP2EN) |
(RCC_PLLCFGR_DIVQ2EN) |
(RCC_PLLCFGR_DIVR2EN));
RCC -> PLLCFGR |= (RCC_PLLCFGR_PLL2VCOSEL_WIDE_RANGE) |
(RCC_PLLCFGR_PLL2RGE_8MHz_16MHz) |
(RCC_PLLCFGR_DIVP2EN) |
(RCC_PLLCFGR_PLL2FRACEN);
RCC -> PLL2DIVR &= ~((RCC_PLL2DIVR_N2) |
(RCC_PLL2DIVR_P2));
RCC -> PLL2DIVR |= (RCC_PLL2DIVR_N2_122) |
(RCC_PLL2DIVR_P2_8);
break;
case 48000:
RCC -> PLLCKSELR &= ~(RCC_PLLCKSELR_DIVM2);
RCC -> PLLCKSELR |= (RCC_PLLCKSELR_DIVM2_DIV4);
RCC -> PLL2FRACR = 0;
RCC -> PLL2FRACR = (RCC_PLL2FRACR_FRACN2_1835);
RCC -> PLLCFGR &= ~((RCC_PLLCFGR_PLL2VCOSEL) |
(RCC_PLLCFGR_PLL2RGE) |
(RCC_PLLCFGR_PLL2FRACEN) |
(RCC_PLLCFGR_DIVP2EN) |
(RCC_PLLCFGR_DIVQ2EN) |
(RCC_PLLCFGR_DIVR2EN));
RCC -> PLLCFGR |= (RCC_PLLCFGR_PLL2VCOSEL_WIDE_RANGE) |
(RCC_PLLCFGR_PLL2RGE_8MHz_16MHz) |
(RCC_PLLCFGR_DIVP2EN) |
(RCC_PLLCFGR_PLL2FRACEN);
RCC -> PLL2DIVR &= ~((RCC_PLL2DIVR_N2) |
(RCC_PLL2DIVR_P2));
RCC -> PLL2DIVR |= (RCC_PLL2DIVR_N2_52) |
(RCC_PLL2DIVR_P2_17);
break;
case 44100:
RCC -> PLLCKSELR &= ~(RCC_PLLCKSELR_DIVM2);
RCC -> PLLCKSELR |= (RCC_PLLCKSELR_DIVM2_DIV4);
RCC -> PLL2FRACR = 0;
RCC -> PLL2FRACR = (RCC_PLL2FRACR_FRACN2_1835);
RCC -> PLLCFGR &= ~((RCC_PLLCFGR_PLL2VCOSEL) |
(RCC_PLLCFGR_PLL2RGE) |
(RCC_PLLCFGR_PLL2FRACEN) |
(RCC_PLLCFGR_DIVP2EN) |
(RCC_PLLCFGR_DIVQ2EN) |
(RCC_PLLCFGR_DIVR2EN));
RCC -> PLLCFGR |= (RCC_PLLCFGR_PLL2VCOSEL_WIDE_RANGE) |
(RCC_PLLCFGR_PLL2RGE_8MHz_16MHz) |
(RCC_PLLCFGR_DIVP2EN) |
(RCC_PLLCFGR_PLL2FRACEN);
RCC -> PLL2DIVR &= ~((RCC_PLL2DIVR_N2) |
(RCC_PLL2DIVR_P2));
RCC -> PLL2DIVR |= (RCC_PLL2DIVR_N2_28) |
(RCC_PLL2DIVR_P2_10);
break;
}
RCC -> D2CCIP1R &= ~(RCC_D2CCIP1R_SPI123SEL);
RCC -> D2CCIP1R |= (RCC_D2CCIP1R_SPI123SEL_PLL2_P_CK);
RCC -> CR &= ~(RCC_CR_PLL2ON);
RCC -> CR |= (RCC_CR_PLL2ON);
while (!((RCC -> CR) & (RCC_CR_PLL2RDY)));
SPI1->I2SCFGR = 0x00;
SPI1->CFG1 &= ~((SPI_CFG1_RXDMAEN) |
(SPI_CFG1_TXDMAEN));
SPI1->CFG1 |= (SPI_CFG1_RXDMAEN) |
(SPI_CFG1_TXDMAEN);
SPI1->I2SCFGR |= (SPI_I2SCFGR_MCKOE) |
(SPI_I2SCFGR_I2SDIV_2) |
(SPI_I2SCFGR_DATFMT_LEFT) |
(SPI_I2SCFGR_I2SSTD_I2S) |
(SPI_I2SCFGR_I2SCFG_MASTER_FULL) |
(SPI_I2SCFGR_I2SMOD_I2S);
switch (INPUT_TYPE) {
case INPUT_INLINE:
//Disable everything else besides INLINE
break;
case INPUT_BLUETOOTH:
//Disable everything else besides BT
break;
}
switch (BIT_RATE) {
case 16:
SPI1->I2SCFGR |= (SPI_I2SCFGR_DATLEN_16BIT);
SPI1->I2SCFGR |= (SPI_I2SCFGR_CHLEN_32BIT);
break;
case 24:
SPI1->I2SCFGR |= (SPI_I2SCFGR_DATLEN_24BIT);
SPI1->I2SCFGR |= (SPI_I2SCFGR_CHLEN_32BIT);
break;
}
DMA1_Stream0->CR |= DMA_SxCR_EN;
DMA1_Stream1->CR |= DMA_SxCR_EN;
SPI1->CR1 |= SPI_CR1_SPE;
SPI1->CR1 |= SPI_CR1_CSTART;
}