Skip to main content
Noirim DIH
Associate II
Jan 25, 2023 7:38 AM UTC
Solved

I2C HAL lock state not properly updated

Hello,

While I was tracking an issue on I2C bus, I found something that seems to be unconsistent in HAL file stm32l4_hal_i2c.c

1 - routines I2C_WaitOn_____UntilTimeout() are called after locking the bus with __HAL_LOCK(hi2c) macro

2- these routines update the lock state in case of error, return and this error to the caller finaly the HAL ends. The caller in that case (error) do not update lock state which is updated by I2C_WaitOn_____UntilTimeout() (=unlock before returning error)

but I found that all path do not update the lock state. for example below the first error do not unlock the bus :

static HAL_StatusTypeDef I2C_WaitOnSTOPFlagUntilTimeout(I2C_HandleTypeDef *hi2c, uint32_t Timeout,

                            uint32_t Tickstart)

{

 while (__HAL_I2C_GET_FLAG(hi2c, I2C_FLAG_STOPF) == RESET)

 {

  /* Check if an error is detected */

  if (I2C_IsErrorOccurred(hi2c, Timeout, Tickstart) != HAL_OK)

  {

   return HAL_ERROR;

  }

  /* Check for the Timeout */

  if (((HAL_GetTick() - Tickstart) > Timeout) || (Timeout == 0U))

  {

   hi2c->ErrorCode |= HAL_I2C_ERROR_TIMEOUT;

   hi2c->State = HAL_I2C_STATE_READY;

   hi2c->Mode = HAL_I2C_MODE_NONE;

   /* Process Unlocked */

   __HAL_UNLOCK(hi2c);

   return HAL_ERROR;

  }

 }

 return HAL_OK;

}

My understanding is that   

/* Process Unlocked */

   __HAL_UNLOCK(hi2c);

is missing before returning the error to the caller. Is it correct?

Regards

This topic has been closed for replies.
Foued_KH
Foued_KHBest answer
ST Employee
May 16, 2023 1:59 PM UTC

Hello @Noirim DIH​ ,

This issue is already fixed : STM32CubeL4/stm32l4xx_hal_i2c.c at c5e83f31696c3da4fb374224471afd08d9d457b3 · STMicroelectronics/STM32CubeL4 · GitHub

Thx

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

Foued_KH
ST Employee
Jan 25, 2023 10:52 AM UTC
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Noirim DIH
Associate II
Jan 25, 2023 11:05 AM UTC

Hello,

thank you for your message. My question is about the code generated by CubeMX which is up to date.

For your information I'm waiting for a fix to this reported issue

https://community.st.com/s/feed/0D53W00001wIeOsSAK

as well.

So I'm using the last available version of CubeMX and generated HAL.

Regards

Foued_KH
Foued_KHBest answer
ST Employee
May 16, 2023 1:59 PM UTC
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.