Skip to main content
MMisa
Associate II
Dec 17, 2019 1:49 PM UTC
Solved

I2C bootloader on STM32G03x problem

I have problem with bootloader on STM32G031. I am using pins PB6 and PB7 according to manual (AN2606), but no response at address 0x51 (I hope Slave 7-bit address: 0b1010001x means 0x51).

I am getting into bootloader by rebooting and remapping SYSCFG_MEMRM to 0x1 in early state. After that I am able to use serial bootloader on pins PA9,PA10 (USART1), but not I2C.

In my user application I2C slave mode is working properly on pins PB6, PB7.

In final application I will have only I2C connection from master system and I will need to reprogramm slave firmware. I was expecting I will use system bootloader.

Is anybody using I2C bootloader on STM32G03x succesfully?

Please give me any advice, how to debug this problem and/or what else I can try.

This topic has been closed for replies.
MMisa
MMisaBest answer
Associate II
Dec 15, 2020 1:09 PM UTC

It seems that is wrong i2c address in the manual - it should be not 0x51, but 0x56. Now I can succesfully detect CPU with the stm32flash software. Unfortunatelly it seems that block erase is not working with the stm32flash tool. I didn't try mass erase and flashing yet (I have calibration values stored in the flash, so I am waiting to new boards for further tests).

1 reply

MMisa
MMisaAuthorBest answer
Associate II
Dec 15, 2020 1:09 PM UTC

It seems that is wrong i2c address in the manual - it should be not 0x51, but 0x56. Now I can succesfully detect CPU with the stm32flash software. Unfortunatelly it seems that block erase is not working with the stm32flash tool. I didn't try mass erase and flashing yet (I have calibration values stored in the flash, so I am waiting to new boards for further tests).