Skip to main content
HSant.1
Associate II
Dec 6, 2021 3:49 PM UTC
Solved

I think I found an error in the ethernet HAL for the STM32F4 , can you confirm ?

The code after the LAN speed auto detection is this :

line 443 @stm32f4xx_hal_eth.c

  if((phyreg & PHY_SPEED_STATUS) == PHY_SPEED_STATUS)

  {  

   /* Set Ethernet speed to 10M following the auto-negotiation */

   (heth->Init).Speed = ETH_SPEED_10M;

  }

  else

  {  

   /* Set Ethernet speed to 100M following the auto-negotiation */

   (heth->Init).Speed = ETH_SPEED_100M;

  }

I think that the speed selection is inverted, I reverse the values and the interface start working

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Dec 6, 2021 4:24 PM UTC

No, the setting depends on the PHY being used. and the value of PHY_SPEED_STATUS.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Dec 6, 2021 4:24 PM UTC

No, the setting depends on the PHY being used. and the value of PHY_SPEED_STATUS.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
HSant.1
HSant.1Author
Associate II
Dec 6, 2021 4:37 PM UTC

Ok, Changing the PHY_SPEED_STATUS solved the problem.

Thanks a lot