Skip to main content
WGril.1
Associate II
Mar 9, 2023 2:56 PM UTC
Question

I'm using STM32H745I and I have problems using ethernet communication.

I'm trying to receive a packet of 15125 bytes. The packet is correctly fragmented in 11 packets, but of each fragment only the first 902 bytes are correct, the rest are equals to 0.

ETH_RX_BUFFER_SIZE: 1536

MEM_ALIGNMENT: 4

MEM_SIZE: 16360

LWIP_RAM_HEAP_POINTER: 0X30044000

MEMP_NUM_REASSDATA: 5

MEMP_NUM_FRAG_PBUF: 30

PBUF_POOL_SIZE: 32

PBUF_POOL_BUFSIZE: 2500

IP_REASS_MAXAGE: 10

IP_REASS_MAX_PBUFS: 50

TCP_MSS: 1460

ETH_RX_DESC_CNT: 15

ETH_TX_DESC_CNT: 4

.lwip_sec (NOLOAD) : {

. = ABSOLUTE (0X30000000);

*(.RxDescripSection)

. = ABSOLUTE (0X30000620);

*(.TxDescripSection)

. = ABSOLUTE (0X30000800);

*(.RxArraySection)

} > RAM_D2

This topic has been closed for replies.

4 replies

Senior II
Mar 9, 2023 3:46 PM UTC
When this account seems to be inactive, try @tdecker2 - ST can't change mail addresses, so I had to create a new account.
WGril.1
WGril.1Author
Associate II
Mar 10, 2023 6:57 AM UTC

It seems to me that everything corresponds to what is described in the guide, except for the MPU. I disabled the MPU.

LCE
Principal III
Mar 9, 2023 4:17 PM UTC

I don't know the H745 SRAM mapping, but are you sure that all that fitting in there where it should?

For the H723..H735 series (which has a different SRAM mapping than the H745) it was mostly important to set the descriptors in SRAM2.

Data and lwIP stuff can be put anywhere except TCM.

I thin the H74x had some limits concerning ETH / AXI RAM, but not sure.

And can you receive smaller packets without error?

WGril.1
WGril.1Author
Associate II
Mar 10, 2023 7:08 AM UTC

This is memories definition:

RAM (xrw) : ORIGIN = 0X24000000, LENGHT = 512K

FLASH (rx) : ORIGIN = 0X08000000, LENGHT = 1024K

DTCRAM (xrw) : ORIGIN = 0X20000000, LENGHT = 128K

RAM_D2 (xrw) : ORIGIN = 0X30000000, LENGHT = 512K

RAM_D3 (xrw) : ORIGIN = 0X38000000, LENGHT = 64K

ITCMRAM (xrw) : ORIGIN = 0X00000000, LENGHT = 64K

I receive correctly smaller packets. There seems to be something limiting the reception as I always correctly receive the same number of bytes