Skip to main content
Desh
Associate
Sep 14, 2022 3:52 AM UTC
Question

I'm having problem with B-L462E-CELL1 evaluation board to connect to truphone network via eSIM in Australia. I'm able to use plastic sim card from telstra to stablish the connection. I'm receiving this error:

AT%CEER?<CR>

  <CR><LF>

  %CEER: 1,"NAS-EMM","ATTACH","REJECT",#15,NO_SUITABLE_CELLS_IN_TRACKING_AREA<CR><LF>

  <CR><LF>

  OK<CR><LF>

Here is the modem configuration:

Cellular Service Infos

Modem state     : 4 (Modem registered on network)

Signal Quality    : 0

Signal level(dBm)  : 0

Operator name    :

IMEI         : 351521100639475

Manuf name      : Murata Manufacturing Co.

Model        : LBAD0XX1SC-DM

Revision       : RK_03_00_00_00_04121_001

Serial Number    : 351521100639475

ICCID        : 8944477300000104512

IMSI         : 208090022802391

Network bearer (AcT) : 0 (GSM)

IP address      : 0.0.0.0

Cellular Service Task State

Current State : WAITING_FOR_NETWORK_STATUS_STATE

Sim Selected : EXTERNAL MODEM SLOT > SIM initialized and ready

All sim information :

- Sim REMOVABLE SLOT : SIM error - too many error rsp during init

  APN :

  APN username :

  APN password :

  APN is sent to modem

- Sim EXTERNAL MODEM SLOT : SIM initialized and ready

  APN : iot.truphone.com

  APN username :

  APN password :

  APN is sent to modem

Cellular Service Task Config

Sim Slot       : 0 (REMOVABLE SLOT)

APN         : ""

CID         : 1

username       :

password       :

Sim Slot       : 1 (EXTERNAL MODEM SLOT)

APN         : "iot.truphone.com"

CID         : 1

username       :

password       :

Attachment timeout  : 180000 ms

nfmc mode      : Not active

Network register mode: 0 = Auto

Access techno present: Not present

$>at at%nwoper="TRUPHONE"

ATParser:*** SEND (size=21) ***

at%nwoper="TRUPHONE"<CR>

<CR><LF>

OK<CR><LF>

I hope someone can help me to resolve this issue.

Thank you all.

This topic has been closed for replies.

3 replies

McLovin
Associate II
Oct 25, 2022 1:19 AM UTC

Same here, also gave up trying Truphone after a while and used Telstra SIM card instead.

Semyalo
Associate II
Jan 6, 2024 8:38 AM UTC

Hi Desh,

I'm also getting started with the BL462E-CELL1. Did your BL462E-CELL1 come with "RK_03_00_00_00_04121_001" as the default modem firmware version? Or you had to update it?

I'm having a challenge of updating the modem firmware version to "RK_03_00_00_00_04121_001" so as to be compliant with the latest X-CUBECELLULAR v7.1.0.

Thanks. 

Semyalo
Associate II
Feb 12, 2024 4:21 PM UTC

With consultation from the muRata support team, the modem factory FW version (RK_03_00_00_00_11851_001) which was pre-installed was compliant with the X-CUBECELLULAR v7.1.0. So, I tested it, and it worked great.