Skip to main content
EKaya.11
Associate
Jan 27, 2022 11:01 AM UTC
Solved

I just want to program my mcu (STM32F103C6T6A) via usb port which is connected to mcu's usb pins. I don't want to use jtag or swd. What should i do for boot0/1 pins?

I read AN2606 but i couldn't understand exactly. My understood is that if i connect boot0 pin to ground, main flash memory is gonna be selected.

My question is if i do it(connecting boot0 pin to ground), will i lose the ability which enable me to program mcu via usb port?.

This topic has been closed for replies.
MM..1
MM..1Best answer
Super User
Jan 27, 2022 1:03 PM UTC

Best hmm

STLINK ??? Is swd HW for program and debug no relevant with bootloader...

And boot0 on ground dont lose ability to run system loader from app, only block boot to.

9 replies

MM..1
Super User
Jan 27, 2022 11:13 AM UTC

You must miss read AN , where you see that 103 have USB DFU? I seent

EKaya.11
EKaya.11Author
Associate
Jan 27, 2022 11:19 AM UTC

But it has usb connection pins. That's why i think like that

MM..1
Super User
Jan 27, 2022 11:22 AM UTC

No this MCU can use only user type DFU. You need split flash to bootloader part and this proggram over SWD or supported boot serial system. After this boot USB and ...

Javier1
Principal
Jan 27, 2022 11:49 AM UTC

>if i do it(connecting boot0 pin to ground), will i lose the ability which enable me to program mcu via usb port?.

You wont be able to use the STLINKs bootloader DFU/UART/...(which requires you to pull high the boot pin after reset)

hit me up in https://www.linkedin.com/in/javiermuñoz/
MM..1
MM..1Best answer
Super User
Jan 27, 2022 1:03 PM UTC

Best hmm

STLINK ??? Is swd HW for program and debug no relevant with bootloader...

And boot0 on ground dont lose ability to run system loader from app, only block boot to.

Javier1
Principal
Jan 27, 2022 2:12 PM UTC

k

hit me up in https://www.linkedin.com/in/javiermuñoz/