I have problems with buffers related to USB endpoints. It seems that data is placed in the wrong buffers or pointer offsets are wrong. I need help to find out what the problem is.
- 1 reply
- 1957 views
Custom HID class device based on the custom HID example.
What I need:
Control endpoint 0 IN
Control endpoint 0 OUT
endpoint 1 IN (0x81)
endpoint 2 OUT (0x02)
endpoint 3 IN (0x83)
endpoint 4 OUT (0x04)
Page 2012 in RM0440: “For this reason, a dedicated feature called ‘double-buffering’ can be used with bulk endpoints.
I want interrupt endpoints - not bulk endpoints. FS devices should support 64 bytes packets and this is what I transmit in my initial tests.
I have set USE_USB_DOUBLE_BUFFER to 0 in stm32g4xx_ll_usb.h.
I allocate 64 Bytes (0x40 bytes) to each endpoint buffer.
The attached files are outputs with different combinations of pmaadress and endpoints conififured as seen below for each output.
Output 1:
In usbd_conf.c, USBD_LL_Init() function I set the following:
/* USER CODE BEGIN EndPoint_Configuration */
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x00 , PCD_SNG_BUF, 0x18);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x80 , PCD_SNG_BUF, 0x58);
/* USER CODE END EndPoint_Configuration */
/* USER CODE BEGIN EndPoint_Configuration_CUSTOM_HID */
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x02, PCD_SNG_BUF, 0x98);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x81, PCD_SNG_BUF, 0xD8);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x04, PCD_SNG_BUF, 0x118);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x83, PCD_SNG_BUF, 0x158);
/* USER CODE END EndPoint_Configuration_CUSTOM_HID */
Output 2:
In usbd_conf.c, USBD_LL_Init() function I set the following:
/* USER CODE BEGIN EndPoint_Configuration */
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x00 , PCD_SNG_BUF, 0x18);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x80 , PCD_SNG_BUF, 0x58);
/* USER CODE END EndPoint_Configuration */
/* USER CODE BEGIN EndPoint_Configuration_CUSTOM_HID */
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x81, PCD_SNG_BUF, 0x98);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x02, PCD_SNG_BUF, 0xD8);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x83, PCD_SNG_BUF, 0x118);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x04, PCD_SNG_BUF, 0x158);
/* USER CODE END EndPoint_Configuration_CUSTOM_HID */
Output 3:
In usbd_conf.c, USBD_LL_Init() function I set the following:
/* USER CODE BEGIN EndPoint_Configuration */
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x00 , PCD_SNG_BUF, 0x18);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x80 , PCD_SNG_BUF, 0x58);
/* USER CODE END EndPoint_Configuration */
/* USER CODE BEGIN EndPoint_Configuration_CUSTOM_HID */
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x82, PCD_SNG_BUF, 0x98);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x01, PCD_SNG_BUF, 0xD8);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x84, PCD_SNG_BUF, 0x118);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x03, PCD_SNG_BUF, 0x158);
/* USER CODE END EndPoint_Configuration_CUSTOM_HID */
Output 4:
In usbd_conf.c, USBD_LL_Init() function I set the following:
/* USER CODE BEGIN EndPoint_Configuration */
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x00 , PCD_SNG_BUF, 0x18);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x80 , PCD_SNG_BUF, 0x58);
/* USER CODE END EndPoint_Configuration */
/* USER CODE BEGIN EndPoint_Configuration_CUSTOM_HID */
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x01, PCD_SNG_BUF, 0x98);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x82, PCD_SNG_BUF, 0xD8);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x03, PCD_SNG_BUF, 0x118);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x84, PCD_SNG_BUF, 0x158);
/* USER CODE END EndPoint_Configuration_CUSTOM_HID */
For output 1 and output 2:
Some buffers have incorrect data or buffer pointers are incorrect.
For output 3 and output 4:
Pipe error