Skip to main content
Einst
Visitor II
Nov 17, 2022 4:46 PM UTC
Question

I have 3 different units running on 3 different stm32 microcontrollers, with all 3 sharing same ground, and I want all 3 boot pins connected together, to enable me to put them all into boot mode with the same input pulse. Is this connection ideal?

..

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Nov 17, 2022 5:58 PM UTC

>>stm32 microcontrollers

Which ones, narrow it down a bit, as there's hundreds, in all sorts of pin configurations.

If just the BOOT0 (INPUT) pin, that isn't collocated with any other functionality / bond-out, then yes they can be driven by a common source.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..