Skip to main content
JJoy.1
Associate III
Aug 9, 2021 10:26 AM UTC
Question

I am using STM32H7A3 board and integrated an SD card using SPI. I am trying to transfer a large file and found that in first card if the number of sector to read is coming as 64, read works upto sector 36.

After 36, it will give error and exited from code.

I tried another card , the code will set the sector count to 16 and loops through it to make the read complete. As i am trying a large file, its taking so much time.

I just want to know, is the sector count ( 16 and 64 for the 2 cards) is solely dependent on card and whether i can change from code. What is the relevance of sector 36 if sector count is 64. Anybody please clarify these things...

Attached code for reference. Above I refer( 64 and 16) the value of cc in file ff.c ( line no.3557)

Thanks,

Jestina

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Aug 9, 2021 5:52 PM UTC

Could it relate to the cluster size being used by the file system on specific cards?

Perhaps look at those via "Properties" in Windows, or the metrics FatFs can provide.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..