Skip to main content
SPate.4
Associate II
Mar 13, 2021 12:26 AM UTC
Question

I am trying to use the FatFs middleware but get stuck in HAL_Delay() when trying to turn the power on to SDMMC. Could someone explain why this might be happening or point to a solution for this. I put the backtrace from gdb in the details.

#0 0x0800add0 in HAL_Delay (Delay=2) at Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal.c:378

#1 0x0800b9ec in SDMMC_PowerState_ON (SDMMCx=0x40012c00)

   at Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_ll_sdmmc.c:316

#2 0x0800c4fe in HAL_SD_InitCard (hsd=0x2000643c <hsd1>) at Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_sd.c:428

#3 0x0800c46c in HAL_SD_Init (hsd=0x2000643c <hsd1>) at Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_sd.c:379

#4 0x08021d9e in BSP_SD_Init () at FATFS/Target/bsp_driver_sd.c:58

#5 0x0800ed46 in SD_initialize (lun=0 '\000') at FATFS/Target/sd_diskio.c:156

#6 0x080169f4 in disk_initialize (pdrv=0 '\000') at Middlewares/Third_Party/FatFs/src/diskio.c:60

#7 0x08019498 in f_mkfs (path=0x20009f5a <SDPath+2> "/", opt=7 '\a', au=0, work=0x2004fdcc, len=512)

   at Middlewares/Third_Party/FatFs/src/ff.c:5334

#8 0x08005a34 in main () at Core/Src/main.c:173

This topic has been closed for replies.

5 replies

SPate.4
SPate.4Author
Associate II
Mar 13, 2021 12:52 AM UTC

I was able to solve this by switching to SysTick for the clock. If anyone knows a solution that doesn't require switching to a SysTick, that would be greatly appreciated.

Tesla DeLorean
Guru
Mar 13, 2021 2:16 AM UTC

Not really much to work with here.

Which TIM vs SysTick?

What are the relative priorities/preempt levels for the interrupts?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Javier1
Principal
Mar 15, 2021 8:30 AM UTC

if you call HAL_delay() inside an interrupt with higher priority than your sistem tick source (systick or tim) it will wait indefinetly for the ticks that will never happen

And effectively stall your program.

hit me up in https://www.linkedin.com/in/javiermuñoz/
Associate II
Jul 7, 2023 9:14 PM UTC

It sounds like that you're using RTOS and calling f_mount function when _FS_REENTRANT macrro is enabled (=1) will call ff_cre_syncobj function is syscall.c to create a new sync. object. If f_mount function is called before RTOS init functions it can cause this type of issue. I would suggest that you move f_mount function into your idle task init section.