Skip to main content
APasi
Associate II
August 20, 2019
Question

I am looking for lwip (or any other) project example runs STM32F767ZI and supports UDP client/server without (!!!) RT operation system

  • August 20, 2019
  • 5 replies
  • 1337 views

Hello'

I'm looking for compact software package that supports UDP/DMA/ETH read/receive data according to the following rules:

  1. Using only LL or HAL (more suitable) functions
  2. OS/RTOS nothing used
  3.  

Thanks in advance for yours assistance,

AlexE

This topic has been closed for replies.

5 replies

Piranha
Principal III
August 20, 2019

Plenty of examples with and without RTOS:

\STM32Cube_FW_F7_V1.15.0\Projects\STM32756G_EVAL\Applications\LwIP

\STM32Cube_FW_F7_V1.15.0\Projects\STM32F769I_EVAL\Applications\LwIP

HAL and "compact" are two opposite terms.

P.S. Reliable, performant and compact lwIP examples fulfill only the 3rd point - they are invisible. :)

APasi
APasiAuthor
Associate II
September 11, 2019

Hello Piranha,

Thank you very much for your answer,

Now I back to the problem...

We changed our platform from F7 to STM32H743ZI and I made new UdpEchoClient application using source STM32H743ZI _EVAL\Applications\LwIP (in other word UdpEchoClient for Nucleo144) without RTOS!

Unfortunately , it doesn't work ...

Maybe you know about any working UdpEchoClient /Server without RTOS (location, download ?

PS: When I try to built trivial Ethernet sample using MX (STM32CubeIDE/MX) it says me that LwIP cannot be attached if RTOS is not enabled - ?

Thanks Alexp

APasi
APasiAuthor
Associate II
September 11, 2019

Hello Piranha,

Thank you very much for your answer,

Now I back to the problem...

We changed our platform from F7 to STM32H743ZI and I made new UdpEchoClient application using source STM32H743ZI _EVAL\Applications\LwIP (in other word UdpEchoClient for Nucleo144) without RTOS!

Unfortunately , it doesn't work ...

Maybe you know about any working UdpEchoClient /Server without RTOS (location, download ?

PS: When I try to built trivial Ethernet sample using MX (STM32CubeIDE/MX) it says me that LwIP cannot be attached if RTOS is not enabled - ?

Thanks Alexp

Piranha
Principal III
September 11, 2019

Why are You posting the same content twice?

Did You read the last sentence of my previous message? There are no publicly available quality STM32 ETH and lwIP driver code! Closest to usable is code from Keil DFP packs and ARM Mbed platform.

But if You need actually working network, then take this as an example and write Your own driver:

https://github.com/lsgunth/lwip_contrib

APasi
APasiAuthor
Associate II
September 11, 2019

Hi Piranha,

1.Yes, I mistook and tried to delete one of two posts, but immediately get something similar ~"You Administrator closed this post and changing .*** ..."

Anyway Sorry(1);

2. Sorry(2) - I didn't understand firstly your sentence "P.S. Reliable, performant and compact lwIP examples fulfill only the 3rd point - they are invisible. " - I new user of ST and it my first project here (after TI)

=)

Thanks