Skip to main content
JHove.1
Associate
Dec 9, 2022 2:45 PM UTC
Question

I am just about to start a journey as embedded software developer, and I am trying to familiarize myself with a STM32L1 discovery kit - the initial feeling is one of bewilderment.

After I successfully attached the board to my laptop and ran the "Press a button to ...." tests my plan was to proceed to the source code of the demo application:

  1. To read through the source code to familiarize with it.
  2. To compile it on my laptop
  3. To flash ti again on the devkit.

I was expecting to find the code e.g. as a zip file or a GitHub repository - but I I can not even find the code? I am most familar with Linux and my intention was to develop on that platform using gcc (arm-none-eabi-gcc)?

This topic has been closed for replies.

12 replies

MM..1
Super User
Dec 9, 2022 3:38 PM UTC
JHove.1
JHove.1Author
Associate
Dec 9, 2022 3:41 PM UTC

Thank you - I have downloaded that and started it successfully - but I still need the source code? Or is it bundled in the IDE?

MM..1
Super User
Dec 9, 2022 4:01 PM UTC

Then open it start new STM32 project wizard and choice your board

0693W00000WKfnMQAT.pngcomplete firmware pack install and empty project ...

Close it and open folder with repository on windows for example

c:\Users\username\STM32Cube\Repository\STM32Cube_FW_L0_V1.12.1\Projects\32L0538DISCOVERY\

here is Demo app, examples and docs.... ofcourse for you L1_V...

JHove.1
JHove.1Author
Associate
Dec 9, 2022 4:05 PM UTC

Thank you for answering. Seems maybe my STM32CubeIDE is not complete?

0693W00000WKfpcQAD.png

JHove.1
JHove.1Author
Associate
Dec 9, 2022 4:35 PM UTC

Got the Stm32CUBE to work - turns out there is a conflict between Wayland and the Eclipse tooling. When I disabled Wayland things worked.

TDK
Dec 10, 2022 12:08 AM UTC

You can load a bunch of examples in STM32CubeIDE with File -> New -> STM32 Project -> Example Selector.

There are also more that can be seen here:

https://github.com/STMicroelectronics/STM32CubeL1/tree/master/Projects

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
Dec 10, 2022 11:02 AM UTC

No concrete examples, but some general thoughts of mine on basics of mcu programming, subject to discussion, here.

JW

S.Ma
Principal
Dec 11, 2022 5:38 AM UTC

Check if there is STM32.support for arduino simpler programming, so your learning goes by levels.

JHove.1
JHove.1Author
Associate
Dec 11, 2022 9:20 AM UTC

Thank you for various answers. An Arduino is on the way.

I must admit I had expected the point of a "Discovery kit" was to provide a quite polished experience, but I guess I'll get there. Right now I am trying to compile the example which was instantiated when I selected the stm32L1 Discory kit. Compilation seems to work - no errors in the console - but when I try to "Run" (whatever that means in this context) I get the following window:

0693W00000WKicqQAD.png

JHove.1
JHove.1Author
Associate
Dec 11, 2022 9:22 AM UTC

Continued:

and when I press the [OK] button I get the following window:

0693W00000WKid0QAD.png

JHove.1
JHove.1Author
Associate
Dec 11, 2022 9:23 AM UTC

I do not really understand what this dialogue wants me to do - but whatever I click on nothing happens. Hard work ;-(