HTTP Server issue
Hello everyone,
I am using an STM32H755ZI-Q Nucleo board and I am trying to run a small test project using an Ethernet connection between my board and my computer.
The goal is to set up a simple HTTP server with two buttons (ON/OFF) that allow me to turn LED3 on and off remotely through a web browser.
However, I am experiencing an inconsistent connection issue. The project only works approximately 1 out of 5 times. Whenever I disconnect the board from my computer and run the code again, the Ethernet connection seems to take too long to establish, preventing the HTTP server from starting properly.
The strange thing is that the exact same code can work perfectly one moment, and then fail a few minutes later after simply disconnecting and reconnecting the board. No changes are made to the code.
Has anyone experienced a similar issue or have any idea what could be causing this behavior?
Any help or suggestions would be greatly appreciated!
Thank you in advance!