Skip to main content
mahmoud boroumand
Associate III
April 29, 2019
Question

How use chan FatFS Library in stm32f030

  • April 29, 2019
  • 1 reply
  • 1272 views

Hello

I use stm32f030k6t6 and i want to read micro sd with chan library.

so i download and use the sample project (http://elm-chan.org/fsw/ff/ffsample.zip)

there is a file named Stm32f100.h on the sample project.if i use other stm32f1xx its work .but when i use stm32f0x its doesn't work and stuck on

CS_HIGH(); /* Set CS# high */

(this line is in the fat_sd_spi.c).

how can i use this library in stm32f030?

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
April 29, 2019

You'll need to do a better job porting the code, the F0 might have a different SPI interface, perhaps watch for the width of the read/write to the DR.

There is an AdaFruit SPI SD card driver in the HAL BSP, along with an SPI driver within the NUCLEO and perhaps other BSPs.

There should be a worked FatFs example for the EVAL series boards. Review the Application tree for the Boards in the CubeF0 repositories.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..