Skip to main content
Associate II
Jun 18, 2024 9:49 AM UTC
Solved

How To Using FMC Write?

I encountered a problem when trying to send more than 5 bytes of data using the FMC.

// impossible example --

#define SD_DATA (*(volatile unsigned char *)0x60000001)

SD_DATA = 0x01;
SD_DATA = 0x02;
SD_DATA = 0x03;
 
Using this method, data is not transmitted to the same address without a delay.
However, it is possible to write data to the FMC if I change the address each time I transmit or use a delay.
 
// possible example -- 1

#define SD_DATA (*(volatile unsigned char *)0x60000001)

SD_DATA = 0x01;
HAL_Delay(1);
SD_DATA = 0x02;
HAL_Delay(1);
SD_DATA = 0x03;
// possible example -- 2

#define SD_DATA1 (*(volatile unsigned char *)0x60000001)
#define SD_DATA2 (*(volatile unsigned char *)0x60000002)
#define SD_DATA3 (*(volatile unsigned char *)0x60000003)
SD_DATA1 = 0x01;
SD_DATA2 = 0x02;
SD_DATA3 = 0x03;
 
What could be the problem?
 
We used the STM32F756, and the following is the FMC initialization.
static void MX_FMC_Init(void)
{
 FMC_NORSRAM_TimingTypeDef Timing;


 /** Perform the NOR1 memory initialization sequence
 */
 hnor1.Instance = FMC_NORSRAM_DEVICE;
 hnor1.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
 /* hnor1.Init */
 hnor1.Init.NSBank = FMC_NORSRAM_BANK1;
 hnor1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
 hnor1.Init.MemoryType = FMC_MEMORY_TYPE_NOR;
 hnor1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_8;
 hnor1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
 hnor1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
 hnor1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
 hnor1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
 hnor1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
 hnor1.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;
 hnor1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;
 hnor1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
 hnor1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;
 hnor1.Init.WriteFifo = FMC_WRITE_FIFO_ENABLE;
 hnor1.Init.PageSize = FMC_PAGE_SIZE_NONE;

/* Timing */
 Timing.AddressSetupTime = 15;
 Timing.AddressHoldTime = 15;
 Timing.DataSetupTime = 31;
 Timing.BusTurnAroundDuration = 8;
 Timing.CLKDivision = 16;
 Timing.DataLatency = 17;
 Timing.AccessMode = FMC_ACCESS_MODE_A;
 /* ExtTiming */

 if (HAL_NOR_Init(&hnor1, &Timing, NULL) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
}
This topic has been closed for replies.
DlakBest answer
Associate II
Jun 27, 2024 1:32 AM UTC

Due to repeated swap errors, I resolved the issue by clearing the cache.

13 replies

mƎALLEm
ST Technical Moderator
Jun 18, 2024 9:58 AM UTC

Hello and welcome to the community.

Please use the button </> to insert your code.

Please read these recommendations on how to post a thread: https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

Thank you for your understanding

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
waclawek.jan
Super User
Jun 18, 2024 12:29 PM UTC

In MPU, set given area to be Device (it's Normal by default, which implies that the processor can merge accesses as it sees fit).

Alternatively, you can use the remap using SYSCFG_MEMRMP.SWP_FMC, the memory area starting at 0xC000'0000 is in MPU set as Device by default.

JW

DlakAuthor
Associate II
Jun 19, 2024 12:29 AM UTC

We used NE1 of the FMC to map the address in the hardware. Does this mean it needs to be remapped to 0xC0000000? What is the reason for mapping to 0xC0000000?

waclawek.jan
Super User
Jun 19, 2024 8:51 AM UTC

> What is the reason for mapping to 0xC0000000?

As I've said above, to have the SRAM in a MPU area tagged as Device. As I've said above, the alternative to remap is to set the SRAM area to Device in MPU.

> but a hard fault occurs

Where? Why? Do you still attempt to write to 0x6000'0000?

Else, debug the hardfault as usually.

JW

 

DlakAuthor
Associate II
Jun 19, 2024 9:19 AM UTC

I wrote the following code and changed all instances of 0x60000000 to 0xC0000000. However, a HardFault is occurring.

ex)

#define ZD_DATA (*(volatile unsigned char *)0xC0000000)
waclawek.jan
Super User
Jun 19, 2024 9:43 AM UTC

You have the FMC properly initialized and the swap performed?

> HardFault is occurring

Where? Single-step in disasm to find out the exact instruction.

JW

 

DlakAuthor
Associate II
Jun 20, 2024 8:59 AM UTC

Upon running, a HardFault occurs immediately.

If I remove the line

SYSCFG->MEMRMP |= SYSCFG_MEMRMP_SWP_FMC_0;

the HardFault disappears.

Even without this code, attempting to access the address 0xC0000000 results in a HardFault.

waclawek.jan
Super User
Jun 20, 2024 1:15 PM UTC

> I have noticed that using BANK1 in FMC_Init causes a hard fault at addresses starting from 0x6000.0000.

After remap, you should not use 0x6000'0000 anymore.

JW

DlakAuthor
Associate II
Jun 24, 2024 12:49 AM UTC

I used 0x6000.0000 before remapping, but if BANK2 is not used during the initialization process, a hard fault occurs. What could be the problem?

waclawek.jan
Super User
Jun 24, 2024 9:28 AM UTC

At this point, I am already lost in what exactly do you do.

Please give us a short summary, what is your actual hardware, what are the FMC settings, and upon which action does the fault occur.

JW

DlakAuthorBest answer
Associate II
Jun 27, 2024 1:32 AM UTC

Due to repeated swap errors, I resolved the issue by clearing the cache.