Skip to main content
Visitor II
Apr 15, 2024 10:29 AM UTC
Question

How to use transfer learning to perform image classification on STM32

How should a new STM32H747I-DISCO be used, why does the display not start after I connect the computer with st-link and display 32kb of memory

This topic has been closed for replies.

1 reply

ST Employee
May 22, 2024 4:36 PM UTC

Hello @beijing,

To prevent ST-Link connection problems, confirm that your development environment is configured for the appropriate target device. Additionally, regularly update the embedded firmware to access new features or corrections. Detailed information is available in the ST-LINK derivatives technical note (TN1235) on st.com.

For proper booting, verify the boot jumpers on the board are set correctly to boot from the designated memory. For detailed guidance on configuring and resolving issues with the display, refer to the STM32H747I-DISCO user manual (UM2411) on st.com.

Thanks and Best Regards,

Dorsaf

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Dor_RH