Skip to main content
Associate III
Nov 1, 2025 12:58 PM UTC
Solved

How to use the “Examples” project in STM32CubeF4 (LTDC_Display_2Layers)

 

Hello,

I am using STM32CubeIDE with the STM32F429I-Discovery board,
and my goal is to connect it with the MT9M001 camera module.
As a first step toward that, I would like to make the LCD display work properly.

In the STM32Cube_FW_F4_V1.28.0 package,
there are many sample projects organized as follows:

 

 
Projects > STM32F429I-Discovery > Examples > LTDC > LTDC_Display_2Layers

 

If I import this Example project into STM32CubeIDE,
will the LCD automatically display the sample image?
Or do I need to perform some additional setup or configuration steps?

I would appreciate any advice or guidance.

This topic has been closed for replies.
Issamos
IssamosBest answer
Super User
Nov 1, 2025 1:43 PM UTC

Hello @chachamaru 

According to the readme.txt file of the example.  After compiling and loading the project. It should display the image without need for any other configuration. 
PS: tested with the RevC of the Boards according to the same readme file.

Best Regards.

II

3 replies

Issamos
IssamosBest answer
Super User
Nov 1, 2025 1:43 PM UTC

Hello @chachamaru 

According to the readme.txt file of the example.  After compiling and loading the project. It should display the image without need for any other configuration. 
PS: tested with the RevC of the Boards according to the same readme file.

Best Regards.

II

Associate III
Nov 4, 2025 3:26 AM UTC

Thank you for your reply.


I was able to get the program running.

MM..1
Super User
Nov 1, 2025 1:50 PM UTC

Reply from @Issamos is true for some revesions DK, but for other not and still exist more as one REV board.