Skip to main content
siungsuestone
Associate
December 24, 2025
Solved

HOW TO USE STM32G4 FMAC ?

  • December 24, 2025
  • 4 replies
  • 710 views

this topic is rare,and i cant find a system learning information,can st develeper friends tell us how to use this peripherals, link to ADC DMA......

Best answer by mƎALLEm

Hello @siungsuestone,

Seems there is no example as you have described: multiple ADC channel conversions outputted to FMAC. You need to read the AN5305 and start your project your self then if you face any issue you can post that in this forum board.

Inspire from the example provided in CubeG4 here (FMAC_Adaptive_FIR_AN5305). It is using a bidimensional array as input to FMAC:

aInputValues[2][ARRAY_SIZE]

Assume you fill that input with ADC conversions.

 

4 replies

KnarfB
Super User
December 24, 2025

try 

AN5305 Application note
Digital filter implementation with the FMAC using STM32CubeG4 MCU Package

hth

KnarfB

siungsuestone
Associate
December 24, 2025

i have read this PDF file,   but i want some file about ADC multiple entrance tWITH FMAC,and some detall point

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
December 24, 2025

Hello @siungsuestone,

Seems there is no example as you have described: multiple ADC channel conversions outputted to FMAC. You need to read the AN5305 and start your project your self then if you face any issue you can post that in this forum board.

Inspire from the example provided in CubeG4 here (FMAC_Adaptive_FIR_AN5305). It is using a bidimensional array as input to FMAC:

aInputValues[2][ARRAY_SIZE]

Assume you fill that input with ADC conversions.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
siungsuestone
Associate
December 24, 2025

when decide to triger HAL_FMAC_FilterPreloadCallback ?OutputThreshold or OutputBufferSize or ExpectedCalculatedFilteredDataSize in AN5305 ? thanks a  lot。。。。