Hello @jumman_JHINGA
Please refer to the MDMA configuration in the example found at 'Projects/STM32H743I-EVAL/Examples/QSPI/QSPI_ReadWriteDual_DMA'.
/*##-4- Configure the DMA channel ###########################################*/
/* Enable MDMA clock */
/* Input MDMA */
/* Set the parameters to be configured */
hmdma.Init.Request = MDMA_REQUEST_QUADSPI_FIFO_TH;
hmdma.Init.TransferTriggerMode = MDMA_BUFFER_TRANSFER;
hmdma.Init.Priority = MDMA_PRIORITY_HIGH;
hmdma.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
hmdma.Init.SourceInc = MDMA_SRC_INC_BYTE;
hmdma.Init.DestinationInc = MDMA_DEST_INC_DISABLE;
hmdma.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE;
hmdma.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE;
hmdma.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE;
hmdma.Init.BufferTransferLength = 4;
hmdma.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE;
hmdma.Init.DestBurst = MDMA_DEST_BURST_SINGLE;
hmdma.Init.SourceBlockAddressOffset = 0;
hmdma.Init.DestBlockAddressOffset = 0;
hmdma.Instance = MDMA_Channel1;
/* Associate the DMA handle */
__HAL_LINKDMA(hqspi, hmdma, hmdma);
/* DeInitialize the MDMA Stream */
HAL_MDMA_DeInit(&hmdma);
/* Initialize the MDMA stream */
HAL_MDMA_Init(&hmdma);
/* Enable and set QuadSPI interrupt to the lowest priority */
HAL_NVIC_SetPriority(MDMA_IRQn, 0x00, 0);
HAL_NVIC_EnableIRQ(MDMA_IRQn);
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om