Skip to main content
Semyalo
Associate II
Jan 6, 2024 7:07 AM UTC
Solved

How to update the modem firmware version on the BL462E-CELL1?

Hi,
I’m using the latest X-CUBECELLULAR version v7.1.0 on the BL462E-CELL1.
However, the modem factory FW version (RK_03_00_00_00_11851_001) isn’t compliant with the X-CUBECELLULAR v7.1.0. 

From the release notes, the X-CUBECELLULAR v7.1.0 requires RK_03_00_00_00_04121_001.
However, I don’t know how and where to download the RK_03_00_00_00_04121_001 modem firmware version.

Your help is much appreciated.
Kind regards.

This topic has been closed for replies.
Semyalo
SemyaloBest answer
Associate II
Feb 12, 2024 4:17 PM UTC

After contacting support from muRata, I was told the modem factory FW version (RK_03_00_00_00_11851_001) is a newer version compared to RK_03_00_00_00_04121_001. So, the “RK_03_00_00_00_11851_001” version works well with the X-CUBECELLULAR version v7.1.0.
I have tested it, and works perfectly.
Regards.

2 replies

Semyalo
SemyaloAuthorBest answer
Associate II
Feb 12, 2024 4:17 PM UTC

After contacting support from muRata, I was told the modem factory FW version (RK_03_00_00_00_11851_001) is a newer version compared to RK_03_00_00_00_04121_001. So, the “RK_03_00_00_00_11851_001” version works well with the X-CUBECELLULAR version v7.1.0.
I have tested it, and works perfectly.
Regards.

Andrew741
Visitor II
Feb 12, 2024 4:21 PM UTC

To download the RK_03_00_00_00_04121_001 modem firmware for your BL462E-CELL1 with X-CUBECELLULAR v7.1.0:

1. Check the official website of the device manufacturer for a downloads or support section.

2. Contact customer support for assistance.

3. Refer to the device's documentation or user manual.

4. Check developer community forums for relevant information.

5. Explore any proprietary update tools provided with the device.

Download firmware from official and trusted sources to ensure compatibility and security. If issues persist, contact the device manufacturer's technical support.