Skip to main content
Er.Anil
Associate II
Jun 28, 2021 6:36 AM UTC
Question

How to transfer 2M Bytes of data via USB-VCP of STM32F429 MCU?

I need to transfer 2 M Bytes of data via USB virtual com port of STM32F429 microcontroller, withing 2-4 seconds.

I am using the USB standard libraries available on ST website. I have successfully transfered small strings, But when it comes to the large data.

This topic has been closed for replies.

3 replies

TDK
Jun 28, 2021 1:12 PM UTC

> I have successfully transfered small strings, But when it comes to the large data.

So why can't you transfer long strings? I should be functionally the same as small string, except you'll need to buffer and wait for the previous transfer to complete before sending more.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Er.Anil
Er.AnilAuthor
Associate II
Jun 30, 2021 4:52 AM UTC

Thank you for replying

Can you tell me which function can be used to check whether precious transfer is complete.

I am using "STM32F USB Drivers & Liberary". So is there any library that contains such a function to check a flag for data transfer complete?

TDK
Jun 30, 2021 4:59 AM UTC