Skip to main content
Wechmarer
Associate
Mar 31, 2022 6:38 PM UTC
Solved

How to switch the DMA buffer in HAL_SPI_Transmit_DMA

While output data from DMA to SPI it should be able to use two buffers. One for the current transfer, one to write data.

But how do I switch between the buffers?

#define BUFFER_SIZE 10
uint8_t txBuffer[BUFFER_SIZE + BUFFER_SIZE];
HAL_SPI_Transmit_DMA(&hspi2, (uint8_t*)txBuffer, BUFFER_SIZE);
 
void HAL_SPI_TxHalfCpltCallback(SPI_HandleTypeDef *hspi)
{
 int value = 0;
 if (txBufferHalf == 0) {
 for (unsigned int i = 0; i < BUFFER_SIZE; ++i) {
 txBuffer[i] = ++value;
 }
 txBufferHalf = 1;
 }
 else
 {
 for (unsigned int i = 0; i < BUFFER_SIZE; ++i) {
 txBuffer[i + BUFFER_SIZE] = ++value + 100;
 }
 txBufferHalf = 0;
 }
}

This topic has been closed for replies.
Wechmarer
WechmarerBest answer
Associate
Mar 31, 2022 7:10 PM UTC

Solved. Has to use both HAL_SPI_TxHalfCpltCallback and HAL_SPI_TxCpltCallback

1 reply

Wechmarer
WechmarerAuthorBest answer
Associate
Mar 31, 2022 7:10 PM UTC

Solved. Has to use both HAL_SPI_TxHalfCpltCallback and HAL_SPI_TxCpltCallback