Skip to main content
AMull.11
Associate III
May 15, 2021 12:09 PM UTC
Question

How to stop the freertos scheduler and execute the code from while of main function?

Hi Guys,

I am working on one of the project using STM32H743, where code will update from the UART.

The Application code is based on the FreeRTOS.

So, when I want to update the firmware i need to stop the FreeRTOS scheduler and get back to the while loop of main function.

I had tried with the vTaskEndScheduler() API, but still code is not coming to while loop of main function.

If any one knows please help me to solve this issue.

Any kind of help will be appreciated.

Thank You.

This topic has been closed for replies.

11 replies

Osto
Senior
May 15, 2021 12:18 PM UTC

Dear AMull,

Its not possible to continue the main. You can stop the scheduler and call your own function to continue with FW update. I don't know the structure of your main function. If there is no call to RTOS functions then you can also call the main yourself.

I hope this helps.

Osto

hs2
Visitor II
May 15, 2021 12:22 PM UTC

Why not using vTaskSuspendAll or disable all interrupts and proceed ? However, it depends on what you want to do (next) in your update procedure.

AMull.11
AMull.11Author
Associate III
May 15, 2021 12:27 PM UTC

Thank you hs2,

Yeah i did that also, still code is not coming t while of main.

In update I just want to store TouchGFX assets in External flash and then i'll jump to the System Bootloader to update the application code.

hs2
Visitor II
May 15, 2021 12:39 PM UTC

You don’t need to go back to main (which is not possible resp. supported). Why do you want that ?

Just stop scheduling (and maybe ISRs by disabling all interrupts) as described before if needed and run the code you want.

AMull.11
AMull.11Author
Associate III
May 15, 2021 12:25 PM UTC

Thank you Osto,

Can give me some inputs how to do this.

Once i get the command to update the firmware then i won't get back to the freertos.

Osto
Senior
May 15, 2021 12:50 PM UTC

When you call ending scheduler or suspend all tasks then your system is like a bare metal system. You can continue your job in the same fuction or call another function to do that. From that time, that's your problem to manage everything at time. The whole system (RTOS related) is frozen but everythig else should work as initialized before supension or you can reinitialize them. You need to stop all activities which has to do with RTOS. Call to such functions would stuck or do nothing or generate exception/faults. In this situation its more luck than knwoledge when its working when you make calls to RTOS. Do nothing which has to do with RTOS. You can still use the CMSIS functions like HAL_Delay instead of xTaskDelay.

I dont know your eaxct situation but normally when I make a firmware update, after success, I reset the system to boot with my new firmware. If you want to start new firmware without reseting the system, thean you need to either uninitialize every thing and call the reset handler yourself or make sure that your firmware deinitialize everything first and then continue with setting everything.

Flashing a new firmware and start RTOS again makes no sense because you have no idea if everything is in the same place as before. The new firmware could have new static variables then the new variable could shift everything few bytes up. Then your new firmware uses locations which dont belongs to the save variables. I wouldn't expect that strongly.

I hope this will answer all you questions. Else please give me more information to help you.

Osto

AMull.11
AMull.11Author
Associate III
May 16, 2021 2:03 PM UTC

Hi Osto, Thank you for info

I will describe brief idea of project,

In this Firmware has Application code, Touch GFX application code and TouchGFX assets.

​

Where Application code and TouchGFX application code has to be store in Internal flash.

And TouchGFX assets has to be store in External Flash.

​

So in Application there is 4 threads.

So when I want to Update the firmware, first I need to update the TouchGFX assets from the Application .

And after that I'll jump to system bootloader, then I'll update the Application code and TouchGFX application code and reset the board the plane new Firmware has to be run.

​

This is actual idea​.

​

But when I want to update the ​TouchGFX assets I want to exit from the freertos and run the one funnction from where I'll update the TouchGFX assets and once it completed then I'll Jump to System bootloader.

​

Give some idea how can I do this, or if you know other way suggest me. ​

Pavel A.
May 15, 2021 4:47 PM UTC

FreeRTOS documentation says that vTaskEndScheduler is implemented only in x86 port.

https://www.freertos.org/a00133.html

--pa

Osto
Senior
May 15, 2021 5:02 PM UTC

You are right. So you can use only vTaskSuspendAll.

AMull.11
AMull.11Author
Associate III
May 16, 2021 2:05 PM UTC

Yeah I used vTaskSuspendAll also, but after doing this how to run one funtion from where I can update the TouchGFX assets I am not getting.

Osto
Senior
May 17, 2021 10:17 AM UTC

Do you update the firmware or datat only? Do you place that data on the same place and has the same length or it differs (including code)?

If you change the code, its absolutley recopmended to reste the system.

If you change data only, then you have to take care that the firmware will work if you change them without compiling the firmware.

If you are not 100.0% sure, then you have to reset the system else you need to start scheduler again and continue work.

I would do: When only data changed then check if the firmware has only eference to the first entry. Then it shure that the firmware can manage the data, even when its changed. I'm almost sure that the Grafik System cant do that. So you have to make a full update and then reset the system. But you cant update the system when you are running the same firmware (in same place). The technik you can use is the IAP (In Application Programming). You place your own boatloader at beginn or at end of the flash and you call the IAP manually. I mean you decide to update the code then you deinitialize everything and either call the IAP manually to update the code or you call the system bootloader. To manage this you can either save in a non volatile RAM area (Battery backupd RAM like RTC RAM) or a special area of normal RAM a special signature. Your Firmware checks this area and if it finds the signature, it starts the firmware update. Afterward this area will be cleared and reset the system. So is IAP working. If you want use the System boot programming its more complicated and need also hardware changes. Specially when the application decides to make update, is the system boot not useable.

You can find the IAP examples on ST web site. They are all using serial interface for update and not available for all MCUs but if you look at them, its very easy to change to another MCU or update to use another way or another protocol.