Skip to main content
SLibe
Associate II
Jan 20, 2020 9:34 PM UTC
Solved

How to retrieve PID (Product ID) from a STM32 MCU using DFU?

We are creating updated versions of our products; existing products are based on STM32F411, the new product versions are based on STM32F446.

We have previously developed a custom firmware update tool - used for field firmware updates by our customers - that runs on Windows; this same tool should work with both the existing product and the new product.

We want to ensure that users do not accidentally load the existing product firmware onto the new products, and vice versa.

We can determine whether the firmware file is for the existing or new product based upon the firmware file name. However, how can we determine whether the DFU target is STM32F411 or STM32F446?

After reading AN2606, it is clear that STM32F411 PID is 0x431, and STM32F446 PID is 0x421. However, all app notes (AN3156, and AN2606) and DfuSe user manuals (UM0384, UM0391, UM0392, UM0412) does not indicate how using the DFU protocol to retrieve the PID.

Simply put - how can we access the PID over DFU from a STM32 MCU?

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jan 21, 2020 1:52 AM UTC

Read DBGMCU_IDCODE @ 0xE0042000 ?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jan 21, 2020 1:52 AM UTC

Read DBGMCU_IDCODE @ 0xE0042000 ?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
SLibe
SLibeAuthor
Associate II
Feb 2, 2020 4:32 AM UTC

Unfortunately, reading 0xE0042000 on these parts returns DFU error code DFU_ERROR (10). And the documentation does not indicate that the External PPB Memory is accessible by the bootloader (the reference manuals for the two parts in question indicate that these are the supported memory areas: Flash, RAM, System Memory, Data Memory, OTP Memory).

Any other ideas?